Last updated: December 3, 2008
This measurement is only applicable to the GSM/GPRS/EGPRS lab applications and a test application with the required feature license.
Set up parameters and measurement results for this measurement are only accessible using the GPIB interface.
The Phase and Amplitude versus Time measurement provides a way to characterize the magnitude and phase errors introduced by the non-linear effects of power amplifiers operating over a wide dynamic range. Measuring the amplitude, phase and frequency as a function of output level makes it possible to create a more accurate output signal by pre-distorting the input signal to the power amplifier.
The Phase and Amplitude versus Time measurement is performed on a continuous wave signal with either a discrete amplitude step waveform (Discrete Waveform Calibration Signal) or continuous ramp waveform (Continuous Waveform Calibration Signal). This measurement requires you to put your mobile station into a test mode that can command the mobile station to generate a waveform, which can be either discrete or continuous.
The Discrete Waveform Calibration Signal may include up to 512 measurement intervals (steps), which can be of varying widths (100 us to 400 ms) and amplitudes (-20 dBm to +35 dBm). For this waveform, you can configure the test set to return different types of results, these are: power, phase, and frequency results (
PCAL
), amplitude and phase pairs (
SAMPle
), or both (
BOTH
). The test set samples the discrete waveform at an effective rate of 156.25 kHz. The results returned by the test set depend on the Result Type parameter setting.
The Continuous Waveform Calibration Signal can be classified as three different waveform types: CONTinuous, CONT2 and CONT3. When the Waveform Type is CONTinuous, the signal required by the test set is a 577us GMSK initial reference burst, followed by a CW signal. The initial reference burst is used to range the expected input power and can be used to trigger the Phase and Amplitude versus Time measurement. The CONT2/CONT3 waveform measures a modulated burst signal (and does not require an initial reference burst). The differences in the way the test set performs measurements on these three waveform types are the effective sampling rate at which the test set returns results and the measurement sample count. For the CONTinuous waveform types, the sampling rate is 1.083 MHz and the maximum count is 5000; for the CONT2 waveform types the sampling rate is 4.333 MHz and the maximum count is 5000; for the CONT3 waveform types the sampling rate is 10 MHz and the maximum count is 50000. The results returned by the test set are amplitude and phase pairs.
This measurement can be armed as a single measurement only. Once triggered, the test set performs a measurement on the mobile generated waveform. The type of measurement and the format of the measurement results depend on the type of waveform (DISCrete, CONTinuous, CONT2, or CONT3) your mobile station generates and, for the DISCrete waveform, the Result Type parameter setting.
Before starting the Phase and Amplitude versus Time measurement, you should first specify the mobile station's
Measurement Frequency
and the
Expected Power Control
on the test set. The Expected Power Level should be set to the maximum power level in the mobile generated waveform, and the RF Generator's cell power should be set to
OFF
. Also before starting, you should specify any waveform specific parameters. See
Configuring a Discrete Waveform Calibration Signal
and
Configuring a Continuous Waveform Calibration Signal
.
The accuracy of this measurement relies heavily on the Spectrum Monitor calibration.
The Phase and Amplitude versus Time measurement is available in all operating modes. However, it is recommended that the operating mode be set to CW mode. CW mode provides the most basic setup for the RF Analyzer (see RFANalyzer ).
It is assumed that the call status is idle since the mobile station must be operating in a test mode to generate the appropriate waveform.
Setup and data output for this measurement is only available via the GPIB commands.
See Calibrating the Phase and Amplitude versus Time Measurement for information on how this measurement is calibrated to ensure accuracy.
For Discrete Waveform Calibration Signals, you must make sure the Interval Count, the number of Interval Centers, and the number of Interval Widths are consistent. The number of returned results depends on the step count. If the number of Interval Centers and/or Interval Widths is less than the step count, invalid data is returned.
This measurement is not concurrent with any other measurements. That is, initiating this measurement automatically aborts any measurement that is currently in progress. Likewise, if any other measurement is initiated, the Phase and Amplitude versus Time measurement is aborted.
This parameter allows you to select the bandwidth filter used for the measurement. The test set provides three types of filter: WIDE, NARRow and ENARrow. You can select the filter type according to the following table. For example, if you want to measure the Power results of a signal with interference out of band, and do not concern much on the test speed, you can select Filter Type
ENARrow
.
Anti-interference ability | Test Speed | Returned Results | |
---|---|---|---|
WIDE | Weak | Fast | Power, phase and frequency |
NARRow | Strong | Slow(*) | Power, phase and frequency |
ENARrow | Strong | Slow(*) | Only Power results are valid. The phase and frequency results are always Nan. |
*When the Filter Type is set to NARRow or ENARrow, the Interval Widths is recommended to be larger than 1ms, which will influence the test speed. |
The GPIB command to set this parameter is SETup:PCALibration:FILTer .
This parameter is only applicable when the
Waveform Type
is
DISCrete
. This is the total number of steps the test set is to measure.
You must make sure the Interval Count, the number of Interval Centers , and the number of Interval Widths are consistent. The number of returned results depends on the step count. If the number of Interval Centers and/or Interval Widths is less than the Interval Count, invalid data is returned.
The GPIB command to set this parameter is SETup:PCALibration:STEP:COUNt .
This parameter is only applicable when the
Waveform Type
is
DISCrete
.This is the time location of the center of each step relative to the time when the trigger event occurs.
The GPIB command to set this parameter is SETup:PCALibration:STEP:CENTer .
This parameter is only applicable when the
Waveform Type
is
DISCrete
.This is the stable portion, or portion you wish to measure, of each power step.
The GPIB command to set this parameter is SETup:PCALibration:STEP:WIDth .
This parameter is only applicable when the
Waveform Type
is
CONTinuous
, CONT2, or
CONT3
. This parameter sets the total number of amplitude and phase samples to be reported by the test set in the Phase and Amplitude versus Time measurement results.
The range of the sample count is:
CONTinuous
or CONT2;
CONT3
.
If you change a CONT3 Measurement to
CONTinuous
or
CONT2
, the count value will be automatically set to 1 if it is originately over 5000. A warning message is popped up to notify the change.
The GPIB command to set this parameter is SETup:PCALibration:MEASurement:COUNt .
This parameter is only applicable when the
Waveform Type
is
CONTinuous
. This parameter is the time the test set waits after the initial reference burst before is starts sampling data to and processing the data into amplitude and phase results.
The GPIB command to set this parameter is SETup:PCALibration:MEASurement:DELay .
This parameter only applicable when the
Waveform Type
is
DISCrete
. This parameter can be set to one of three options:
PCAL
,
SAMPle
, or
BOTH
. The setting for this parameter determines what type of measurement results the test set returns after measuring the Discrete Waveform Calibration Signal. For information on the type of results the test set returns base on the setting of this parameter, see
Phase and Amplitude Measurement Results for a Discrete Waveform
.
The GPIB command to set this parameter is SETup:PCALibration:RESult:TYPE .
You can set the timeout state and time for this measurement. To set them separately, use SETup:PCALibration:TIMeout:STATe to set the timeout state, SETup:PCALibration:TIMeout:TIME to set the timeout time, or SETup:PCALibration:TIMeout:STIMe to set the state and time using the complex command.
This is the specified time between the trigger event and when the test set begins sampling data.
The range of the trigger delay is:
If you change a CONT2 /CONT3 Measurement to DISCrete or CONTinuous, the trigger delay will be automatically set to zero if it is originately negative. A warning message is popped up to notify the change.
The GPIB command to set this parameter is SETup:PCALibration:TRIGger:DELay .
You can set the Trigger Source to
IMMediate
,
RISE
(RF Rise), or
EXTernal
. See
Triggering of Measurements
.
The GPIB command to set this parameter is SETup:PCALibration:TRIGger:SOURce .
This is the level below the maximum power level (the power level of the initial reference burst) at which the measurement triggers. That is, the trigger threshold is the offset below the Expected Input Power plus the RF Amplitude Offset value. This parameter only applies if the Trigger Source is set to RISE.
The GPIB command to set this parameter is SETup:PCALibration:TRIGger:THReshold .
This parameter classifies the characteristics of the calibration signal generated by the mobile station. The settings available for this parameter are DISCrete, CONTinuous, CONT2, or CONT3. See Configuring a Discrete Waveform Calibration Signal and Configuring a Continuous Waveform Calibration Signal for more information.
Note, for certain feature licenses the waveform type must be set to CONT2 or CONT3 to initiate the measurement.
The GPIB command to set this parameter is SETup:PCALibration:WAVeform:TYPE .
A discrete waveform consists of a sequence of up to 512 measurement intervals (steps), which be of varying widths (between 100 us and 400 ms) and amplitude levels (-20 dBM to +35 dBM). All steps in a discrete waveform must be at the same carrier frequency.
The total sampling time is the largest Interval Center plus half of the corresponding Interval Width. The maximum sampling time is 400 ms. Therefore if the largest Interval Center plus half of the corresponding Interval Width exceeds 400 ms, the test set returns integrity indicator 21 (Parameter Error).
The maximum power setting is used to range the measurement and can be used as the reference for the trigger level, which is set by configuring the Trigger Threshold parameter. The Trigger Delay should also be configured prior to measuring the waveform. A wait is needed after the measurement initiates and before the waveform's RF Rise trigger event occurs.
If the Result Type is set to
PCAL
, there are parameters specific to the discrete waveform that you should set prior to measuring the discrete waveform. These parameters are necessary to completely define where the test set makes measurements on the discrete waveform, these are:
Interval Count
,
Interval Centers
, and
Interval Widths
.
The figure below is an example of a Discrete Waveform calibration signal when the Result Type parameter is set to
PCAL
.
The test set samples the discrete waveform at an effective rate of 156.25 kHz. These format of the results returned by depend on the Result Type parameter. See Phase and Amplitude Measurement Results for a Discrete Waveform for details on what the test set returns after performing the Phase and Amplitude versus Time measurement on a discrete waveform calibration signal generated from a mobile station.
If you wish to measure a continuous signal, the
Waveform Type
should be set to
CONTinuous
, CONT2,
or
CONT3
. The CONTinuous waveform must consist of a GSM burst followed by the waveform to be measured. For the test set to trigger properly, the Initial Reference Burst (GSM burst) should be at the maximum power level of the waveform. The CONT2 and CONT3 waveforms both do not require the Initial Reference Burst.
NOTE: When measuring a
CONT2
or CONT3 waveform, and the
Trigger Source
is set to
RISE
, the waveform must begin with a sharp rise toward the maximum power setting in order for the test set to trigger. The measurement will not trigger until the power level rises above the
Trigger Threshold
.
The Expected Power Control parameter in the test set should be set to the maximum power level. This setting is used to range the measurement and can be used as the reference for the trigger threshold, which is set by configuring the Trigger Threshold parameter. A wait is needed after the measurement initiates and before the waveform's trigger event occurs.
The figure below shows an example of a
CONTinuous
waveform (including the required Initial Reference Burst). The Waveform Type parameter determines the effective sampling rate used for the continuous waveform. For the
CONTinuous
waveform types, the sampling rate is 1.083 MHz, and for
CONT2
waveform types the sampling rate is 4.333 MHz, while the sampling rate for the
CONT3
waveform types is 10 MHz. You should specify the
Measurement Sample Count
,
Trigger Delay
, and
Measurement Delay
parameters before you measure the continuous waveform.
See Phase and Amplitude versus Time Measurement Results for a Continuous Waveform to learn what values the test set returns after performing the Phase and Amplitude measurement on a continuous waveform calibration signal generated from a mobile station.
The test set returns the Phase and Amplitude versus Time measurement results via the GPIB interface only. The Phase and Amplitude versus Time measurement results depend on the mobile generated waveform type.
If the waveform you are measuring is a discrete waveform, see Phase and Amplitude Measurement Results for a Discrete Waveform .
If the waveform you are measuring is a continuous waveform, see Phase and Amplitude versus Time Measurement Results for a Continuous Waveform .
This section only applies when the Waveform Type parameter is set to
DISCrete
.
You can configure the test set to return Phase and Amplitude versus Time measurement results in three different formats (result types):
This section only applies when the Result Type parameter is set to
PCAL,
and when the Waveform Type is Discrete.
The results that the test set returns are an integrity indicator for the entire measurement, followed by power, phase, and frequency measurement results for specified intervals. The power, phase, and frequency results for the first measurement interval are slightly different than the rest. The first measured power result is an absolute power measurement, the first phase result is set to 0×, and the first frequency result is the offset relative the expected input frequency (which is set using the GPIB command RFANalyzer:MANual:MEASurement[:MFRequency] ). A negative frequency result indicates the first measurement interval is below the expected input frequency, and a positive result indicates the first measurement interval is above the expected input frequency.)
The results from the first measurement interval are returned as the first element in the returned power, phase and frequency arrays, respectively. All subsequent measurement results are relative to the results of the first measurement interval. Therefore, the results of the measured power level, phase, and frequency of the second measurement interval are given relative to the power level, phase, and frequency of the first measurement interval.
The Phase and Amplitude versus Time measurement completes without returning a 5 (Over Range) or 6 (Under Range) integrity indicator as long as the measured power is within +/-6 dB of the expected power for that burst. However, measurement accuracy is warranted only if the measured power is within 3 dB of the expected power.
All results returned from the test set in the power, phase, and frequency arrays are measured relative to the measurement results of the initial measurement interval. If you send a GPIB query for all the results, the results are returned in the following order: integrity indicator, power measurement results array, phase measurement results array, and frequency measurement results array. Alternatively, you can independently query the test set for the integrity indicator, or any of the individual result arrays. The maximum power, phase, and frequency array size the test set returns is 512.
The GPIB query to retrieve the results from the test set a listed in the following table.
GPIB Query | |
---|---|
Measurement Integrity Indicator | FETCh:PCALibration:INTegrity? |
FETCh:PCALibration:POWer? | |
FETCh:PCALibration:PHASe? | |
FETCh:PCALibration:FERRor? | |
All (Integrity Indicator, Power Array, Phase Array, Frequency Array) | READ:PCALibration[:ALL]? or FETCh:PCALibration[:ALL]? |
This section only applies when the Result Type parameter is set to
SAMPle
, and the Waveform Type is
DISCrete
., or when the Waveform Type is
CONTinuous
or
CONT2
.
There is one integrity indicator for the entire measurement. The Phase and Amplitude versus Time measurement completes without returning a 5 (Over Range) or 6 (Under Range) integrity indicator as long as the measured power is within +/-6 dB of the expected power for that burst. However, measurement accuracy is warranted only if the measured power is within 3 dB of the expected power. You can obtain this result using the FETCh:PCALibration:INTegrity? command.
The following values are returned by the test set for each sample point.
You can obtain these results using the FETCh:PCALibration:SAMPle:AMPLitude? <range> command.
*If you wish to convert the data results to have units of mW, you must square the data results. For example, if the test set returns an amplitude value of 10 this corresponds to 100 mW (since 10^2=100). Alternatively, if you wish to convert the data results to have the units of dBm, you must use the formula 20*log10(normalized voltage). For example if the test set returns an amplitude value of 10 this corresponds to 20 dBm (since 20*log10(10)=20).
You can obtain these results using the FETCh:PCALibration:SAMPle:PHASe? <range> command.
The Amplitude and Phase results are returned in groups of 1000 amplitude and phase pairs. The Measurement Sample Count (total number of amplitude and phase pairs) can be queried using the command FETCh:PCALibration:SAMPle:COUNt? . Therefore, the total number of groups that the results are divided among is the (Measurement Sample Count plus 0.5)/1000 rounded up to the nearest integer value. (Where the 0.5, or half a pair, is due to the integrity indicator.) The maximum Measurement Sample Count is 5000.
This section only applies when the Result Type parameter is set to
BOTH
, and the Waveform Type is
DISCrete.
This result type is a combination of the PCAL and Sample result types. The following values are returned by the test set:
This section is only applicable when the Waveform Type is
CONTinuous
,
CONT2
. or
CONT3
The Phase and Amplitude versus Time measurement results for a Continuous Waveform Calibration Signal are returned in the same format as the results for a Discrete Waveform Calibration Signal when the Result Type is set to SAMPle.
See Sample Measurement Results for more information on what measurement results the test set returns for a Continuous Waveform Calibration Signal.
For more information see Integrity Indicator .
The Phase and Amplitude versus Time measurement has the following input signal requirements:
This measurement automatically calibrates the phase and amplitude results when the waveform type is DISCrete or CONTinuous. However, to ensure triggering accuracy when the trigger source is set to RF Rise, you must run the Spectrum Monitor Calibration at least once a month.
This measurement is not automatically calibrated when the waveform type is CONT2 or CONT3; it relies on the Spectrum Monitor calibration factors.
See Recommended Calibration Intervals for more information on when the Spectrum Monitor calibration should be performed.
Programming a Phase and Amplitude vs. Time Measurement (Discrete Waveform)
Programming a Phase and Amplitude vs. Time Measurement (CONTinuous Waveform)
Programming a Phase and Amplitude vs. Time Measurement (CONT2 Waveform)