Last updated: December 3, 2008
The process for making a base station originated call is to:
If necessary, configure the traffic channel parameters for the call assignment. See CALL:TCHannel .
If necessary, set the IMSI state. See CALL:PAGing:IMSI .
If necessary, set the repeat paging state. See CALL:PAGing:REPeat[:STATe][:SELected] .
Configure the necessary call processing connect/disconnect synchronization conditions.
See
Call Processing State Synchronization
.
Page the mobile station by sending the call originate command to the test set.
The process for making a mobile station originated call is to:
If necessary, configure the traffic channel parameters for the call assignment. See CALL:TCHannel for more information about the traffic channel parameters.
Configure the necessary call processing connect/disconnect synchronization conditions.
See
Call Processing State Synchronization
.
Initiate a call from the mobile station.
The test set must be in active cell operating mode and the connection type must be Auto. The correct frequency band must be selected.