Last updated: December 3, 2008
This section is only applicable to EGPRS.
The following procedure assumes that the mobile station is connected to the test set's RF IN/OUT connector.
10 ! Turn the cell off to access the serving cell parameter 20 OUTPUT 714;"CALL:OPER:MODE OFF" 30 ! Change the serving cell to EGPRS 40 OUTPUT 714;"CALL:BCH:SCEL EGPRS" 50 ! Turn the cell back on 60 OUTPUT 714;"CALL:OPER:MODE CALL" 70 ! Set the connection type to ETSI Type A 80 OUTPUT 714;"CALL:FUNC:CONN:TYPE A" 90 ! Select a Modulation and Coding Scheme using 8PSK 100 OUTPUT 714;"CALL:PDTCH:MCSC MCS9,MCS9" 110 OUTPUT 714;"SET:EMAC:CONT OFF"!Set trigger mode to single 120 OUTPUT 714;"SET:EMAC:COUN 5"! Turn statisical results on 130 ! Turn measurement timeout on and set to 5 seconds 140 OUTPUT 714;"SET:EMAC:TIM 5" 150 ! 160 !!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!! 170 ! Turn on the mobile station and allow it to attach 180 !!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!! 190 ! 200 ! Start the data connection 210 OUTPUT 714;"CALL:FUNC:DATA:START" 220 ! Hanging query to determine when the data connection 230 ! has been established. 240 OUTPUT 714;"CALL:TRAN?" 250 ENTER 714;Tran_state 260 IF NOT Tran_state THEN 270 PRINT "DATA CONNECTION FAILED" 280 STOP 290 END IF 300 OUTPUT 714;"INIT:EMAC" ! Initiate measurement 310 ! The query below fetches the measurement results required 320 ! by the conformance specification for modulation accuracy. 330 OUTPUT 714;"FETC:EMAC:ETSI?"! Fetch measurement results 340 ENTER 714;Integrity,Rms_evm,Peak_evm,Percentile,Ferr,Origin_offset 350 END
The measurements returned by the FETCh? query in the programming example above are:
Integrity
returns the measurement
Integrity Indicator
(0 means a successful measurement with no errors).
Rms_evm
returns the RMS Error Vector Magnitude in percent.
Peak_evm
returns the Peak Error Vector Magnitude in percent.
Percentile
returns the 95th Percentile Error Vector Magnitude in percent.
Origin_offset
returns the origin offset suppression in dB.Modulation Accuracy Measurement Description
How do I make Modulation Accuracy Measurements?