AMR Setup

Last updated: October 30, 2013

AMR Source

The following AMR Sources are available in the test set:

GPIB command: CALL:SERVice:AMR:SOURce

This parameter can only be set when call/data status is idle.

AMR Radio Access Bearer

The AMR Radio Access Bearer can be set to:

GPIB command: CALL:SERVice:AMR:RAB

This parameter can only be set when call/data status is idle. Note: "k" refers to kbps.

AMR Voice SRB

This setting specifies the data rate of DCCH used for AMR voice connection when AMR Radio Access Bearer is set to 5.15k Voice or 4.75k Voice .

GPIB command: CALL:SERVice:AMR:SRB

This parameter can not be changed in Active Cell operating mode and the Call/Data Status is not Idle .

Related Topics


Manual Operation: How Do I Configure the AMR Radio Access Bearer?

AMR Voice Ladder Diagrams

Downlink Channel Codes and Levels

Current Service Type

Establishing a Connection with the UE

Paging Service