CW Operating Mode

CW Operating Mode

January 15, 2009

Description

When in CW operating mode, the test set operates like a signal generator. The basic features provided by CW operating mode are:

Test Signals Description

The test set in CW operating mode provides any one of three test signals: CW (no modulation), AM (fixed 56% amplitude modulation), and DSB-SC (dual side-band suppressed carrier). An example usage of the test signals is for calibrating mobile stations that use Qualcomm's radioOne™ Zero Intermediate Frequency (Zero IF) architecture.

You can select any one of three signals with adjustable power level and frequency for output to the currently selected front panel RF connector.

  • With CW test signal selected (the default setting), the test set provides an unmodulated carrier. With either AM or DSB-SC test signal selected, the test set will modulate the signal as shown in the following figure.
  • For any of the test signals selected, the output power level is controlled by the Cell Power ( F7 ). The Cell Power refers to the power found in the entire signal including sidebands if applicable.
  • For any of the test signals selected, the frequency is adjusted by changing the RF Gen Freq ( F8 ).
    • With the CW or AM signal selected, the RF Gen Freq setting represents the center frequency of the signal (fc).
    • With the DSB-SC signal selected, the RF Gen Freq setting represents the frequency of the lower sideband signal (fL). The upper sideband (fh) is 20 kHz above the RF Gen Freq setting, that is fh = fL+20 kHz.

Programming Usage

Use the following commands to control each function for CW operating mode:

Calibrating the Test Set

See Burst Mod Offset 1 Calibration .

Related Topics


Effects on Receiver Control When Changing Operating Mode

Active Cell Operating Mode

Triggering of Measurements