Current Service Type

Current Service Type

Last updated: March 3, 2009

Current Service Type indicates the type of service that is currently active. While in Active Cell Operating Mode , Current Service Type is displayed on the Call Setup Screen (and can be queried using the CALL:STATus:SERVice:TYPe? command). Current Service Type is set to the active service type upon completion of the establishment of the service.

The test set supports the following service types:

Current Service Type is set to None whenever an event occurs that causes the service to be stopped. For example:

Related Topics


Establishing a Connection with the UE

Paging Service

CALL:STATus:SERVice:TYPe?