Call Processing Status

Call Processing Status

Last updated: January 15, 2009

Call Processing Status

The Call Processing Status window on the Call Setup screen displays the following information when in Active Cell Operating Mode :

Active Cell Connection State

Additional call processing state information is also displayed in the small Active Cell window at the bottom of the Call Setup screen. Note that for single services, the respective Call Connection State or Data Connection State is displayed. When Simultaneous Services is active the Active Cell window displays both the call connection state and the data connection state (in that order) separated by a "/".

Call Connection State

The call connection state can transition between the following states:

GPIB commands: CALL:STATus[:STATe][:VOICe]? and CALL:CONNected[:STATe]

Data Connection State

The data connection state can transition between the following states:

GPIB command: CALL:STATus[:STATe]:DATA?

Related Topics


CALL:STATus

CALL:CONNected

Call Processing State Synchronization

Instrument Status Area