Last Updated: January 15, 2009
When the test set is operated remotely, all of the keys on the front panel of the test set are disabled (except the LOCAL key and the power switch). During remote operation the test set is controlled by the Remote User Interface, (RUI).
Any open menus are be closed, and any manual entries are be aborted when the test set transitions from local mode to remote mode.
The remote annunciator (R) will appear in the Instrument Status Area of the test set's display indicating that the test set is in remote mode.
When the test set is in remote mode press the LOCAL key on the front panel in order to gain manual control.