The test set provides up to ten save/recall registers. Each register is identified by a number (1-10).
This section details the following:
Press the Register recall hardkey.
Use the knob to scroll to a register that is labeled Full and press the knob.
When a register is recalled, the test set will clear all active measurements and display the Call Setup Screen. Registers can only be recalled in the format they were saved in. For example, in a fast switching application, a register that is saved in a specific format must also be recalled in that same format. If a register is attempted to be recalled in a format other than the one it was saved in, the following error will occur:
Pressing the DELETE hardkey will display a menu indicating which registers have been saved (they are labeled "Full").
Use the knob to scroll to a register and press the knob. Select Yes to confirm the selection.
All functions and parameters that have an associated static state or settable value will be saved. For example:
Functions that trigger immediate actions, such as originating a call or calibrating a measurement are not saved.
Settings saved in non-volatile memory (settings that are unchanged when power is cycled or the test set is preset) are not saved. For example:
Read-only call processing results such as Mobile Station Information tables are not saved.
To save the current state of the test set, press the SAVE hardkey.
A menu will be displayed that shows the status of all five registers. If the register status is "Full", the register has had instrument settings saved to it. If the register status is "Empty", it does not currently contain any instrument settings.
Use the knob to scroll to a register and press the knob. If the selected register is currently Full, select Yes in the Overwrite Save Reg? window and it will be overwritten.
When the
Save
hardkey is pressed, you can also set a name for each register to easily identify your saved configuration.To set a name for a specific register, press the
Save
hardkey. The Save Registers menu is displayed for you to operate on each register. Highlight the register you want to allocate a name, press the
Set Register Name
softkey on the left, a middle menu is displayed for you to edit the register name.
You can set the register name with a maximum length of 20 characters.
Once you have assigned a name to the register, the name will be in parentheses after the register number.