CALL:CPC

CALL:CPC

Last updated: January 6, 2012

GPIB Command Conventions

CALL:CPC:CQI:DTX:TIMer

Function

Sets/queries the CQI DTX Timer.

This parameter impacts the CQI reporting reduction functionality for UL DTX operation and defines the time duration in subframe unit after a downlink HS-DSCH reception during which the CQI reports have higher priority than the UL DTX pattern and are transmitted according to the regular CQI reporting pattern defined by CQI Feedback Cycle and CQI Repetition Factor. In particular the value "Infinite" provides the network with a chance to disable the CQI reporting reduction functionality at the UE side when running UL DTX operation.

Setting

Range: SUBFrames0|SUBFrames1|SUBFrames2|SUBFrames4|SUBFrames8|SUBFrames16| SUBFrames32|SUBFrames64|SUBFrames128|SUBFrames256|SUBFrames512|INFinite

Query

SUBF0|SUBF1|SUBF2|SUBF4|SUBF8|SUBF16|SUBF32|SUBF64|SUBF128|SUBF256|SUBF512|INF
*RST Setting SUBFrames32
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:CQI:DTX:TIMer SUBFrames32"

CALL:CPC:DRX:ORDer

Function

Sets/queries the DRX Order Info.

This setting is used to configure which order will be sent on HS-SCCH to control the DL DRX operation on the air after DL DRX has been configured to UE. Based on coding rules in 3GPP 25.212 v790 section 4.6C, 0 corresponds to a DL DRX deactivation order, while 1 corresponds to a DL DRX activation order.

Setting

Range: 1|0

Query

Range: 1|0

*RST Setting

0

Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:DRX:ORDer 0"
! Configures a DL DRX deactivation order.

CALL:CPC:DTX:ORDer

Function

Sets/queries the DTX Order Info.

This setting is used to configure which order will be sent on HS-SCCH to control the UL DTX operation on the air after UL DTX has been configured to UE. Based on coding rules in 3GPP 25.212 v790 section 4.6C, 0 corresponds to an UL DTX deactivation order, while 1 corresponds to an UL DTX activation order.

Setting

Range: 1|0

Query

Range: 1|0

*RST Setting

0

Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:DTX:ORDer 0"
! Configures a DL DTX deactivation order.

CALL:CPC:ENABling:DELay

Function

Sets/queries the Enabling Delay.

This parameter is common for UL DTX and DL DRX operation and defines an UL DTX or UL DTX + DL DRX activation delay after the network has configured the corresponding operation to the UE, this delay period allows for the stable synchronization and power control loop between UE and network.

Setting

Range: FRAMes0|FRAMes1|FRAMes2|FRAMes4|FRAMes8|FRAMes16|FRAMes32|FRAMes64|FRAMes128

Query

Range: FRAM0|FRAM1|FRAM2|FRAM4|FRAM8|FRAM16|FRAM32|FRAM64|FRAM128

*RST Setting FRAMes0
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:ENABling:DELay FRAMes0"

CALL:CPC:HLESs:HSPDschannel:CODE[:SECond]

Function

Sets/queries the HS-PDSCH Second Code Support.

The standard specifies that at most two predefined HS-PDSCH codes are assigned per UE for HS-SCCH-less operation. The four comma-separated value indicates whether the second HS-PDSCH code will be used for the corresponding TB size indexed by CALL:CPC:HLESs:TBSize:INDex . "1" means that two HS-PDSCH codes will be used for the corresponding transport block, otherwise only one HS-PDSCH code will be used.

This setting is only applicable when the Current HS-SCCH-less Activated State is On and the HS-DSCH Transmission Type is "HS-SCCH-less".

Setting

4 comma separated values in the range: 1|0

Query

4 comma separated values in the range: 1|0
*RST Setting 0, 0, 0, 0
Requirements

Lab Application Revision: F.01 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:HLESs:HSPDschannel:CODE 0, 0, 0, 0"

CALL:CPC:HLESs:NTRans

Function

Sets/queries the HS-SCCH-less Number of Transmission.

This setting controls the number of times a predefined transport block will be transmitted for the HS-SCCH-less operation.

Setting

Range: 1 to 3

Query

Same as setting
*RST Setting 2
Requirements Lab Application Revision: F.01 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:HLESs:NTRans 2"

CALL:CPC:HLESs:ORDer

Function

Sets/queries the "HS-SCCH Less Order Info" .

This setting is used to configure which order will be sent on HS-SCCH to control the HS-SCCH less operation on the air after HS-SCCH less operation has been configured to UE. In accordance with the standard 3GPP 25.212, 0 corresponds to an HS-SCCH less deactivation order, while 1 corresponds to an HSSCCH less activation order.

This setting is not available when the CPC Mode is set to UL DTX or UL DTX + DL DRX .

Setting

Range: 0 | 1

Query

Same as setting
*RST Setting 0
Requirements Lab Application Revision: G.00.00 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:HLESs:ORDer?"

CALL:CPC:HLESs:TBSize:INDex

Function

Sets/queries the HS-SCCH-less TB Size Index.

Based on the specification, up to 4 transport block formats can be predefined for HS-SCCH-less operation in terms of transport block size and the HS-PDSCH codes used for this transport block transmission. Each entry in this list defines the index of a HS-DSCH transport block size that will be configured for HS-SCCH-less operation.

Setting

Up to 4 comma separated values in the range: 0 to 90.

Query

Same as setting
*RST Setting 20, 0, 0 ,0
Requirements Lab Application Revision: F.01 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:HLESs:TBSize:INDex 20, 0, 0, 0"

CALL:CPC:HSDSchannel:TTYPe

Function

Sets/queries the HS-DSCH Transmission Type. This setting is used to switch the HSDSCH transmission type after HS-SCCH-less operation has been enabled.

Setting

Range: HLESs|HSSCch

Query

Range: HLES|HSSC

*RST Setting HLESs
Requirements Lab Application Revision: F.01 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:HSDSchannel:TTYPe HLESs"

CALL:CPC:HSSCchannel:ORDer:FROM

Function

This parameter controls which cell is used to send the HS-SCCH Order to activate/deactivate the DTX and DRX based on DTX Order Info and DRX Order Info .

Setting

Range: SCELl |SSCell | ALL

Query

Same as setting

RST Setting

ALL

Requirements

Test Application Revision: A.19.00 and above, with the required feature license.
Lab Application Revision: H.01.00.

Programming Example

 
OUTPUT 714;"CALL:CPC:HSSCchannel:ORDer:FROM SSCell" 
!Sets the Secondary Serving Cell to send the HS-SCCH Order to activate/deactivate the DTX and DRX.

CALL:CPC:HSSCchannel:ORDer:SEND[:IMMediate]

Function

Perform the Send HS-SCCH Order action.

Requirements

Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:HSSCchannel:ORDer:SEND" 
!Initiates a Send HS-SCCH Order.

CALL:CPC:MAC:DTX:CYCLe[:MS10]

Function

Sets/queries the MAC DTX Cycle (10ms TTI).

This parameter defines the pattern of time instances at the start of new uplink EDCH transmission after an E-DCH inactive period is allowed when E-DCH TTI is 10ms. This E-DCH inactive period is defined by the "MAC Inactivity Threshold" parameter.

Setting

Range: SUBFrames5|SUBFrames10|SUBFrames20

Query

Range: SUBF5|SUBF10|SUBF20

*RST Setting SUBFrames10
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MAC:DTX:CYCLe SUBFrames10"

CALL:CPC:MAC:DTX:CYCLe:MS2

Function

Sets/queries the MAC DTX Cycle (2ms TTI).

This parameter defines the pattern of time instances where the start of new uplink EDCH transmission after an E-DCH inactive period is allowed when E-DCH TTI is 2ms, this E-DCH inactive period is defined by the "MAC Inactivity Threshold" parameter.

Setting

Range: SUBFrames1|SUBFrames4|SUBFrames5|SUBFrames8|SUBFrames10|SUBFrames16|SUBFrames20

Query

Range: SUBF1|SUBF4|SUBF5|SUBF8|SUBF10|SUBF16|SUBF20

*RST Setting SUBFrames8
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MAC:DTX:CYCLe:MS2 SUBFrames8"

CALL:CPC:MAC:ITHReshold

Function

Sets/queries the MAC Inactivity Threshold.

This parameter impacts the functionality of the UL DRX at NodeB when running a UL DTX operation and is used to define the E-DCH inactive period after which the UE can only start a new E-DCH transmission at given time instances controlled by the "MAC DTX Cycle (10ms TTI)" or "MAC DTX Cycle (2ms TTI)". The E-DCH inactive period is in E-DCH TTI units based on the value of the "HSUPA TTI Mode" parameter.The value "Infinite" allows the network to disable the UL DRX at NodeB functionality, which will introduce the negative impact on NodeB processing resource saving within the UL DTX context.

Setting

Range: ETTis1|ETTis2|ETTis4|ETTis8|ETTis16|ETTis32|ETTis64|ETTis128|ETTis256|ETTis512|INFinite

Query

Range: ETT1|ETT2|ETT4|ETT8|ETT16|ETT32|ETT64|ETT128|ETT256|ETT512|INF

*RST Setting ETTis8
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MAC:ITHReshold ETTis8"

CALL:CPC:MODE

Function

Sets/queries the CPC Operation Control.

This setting controls the CPC operation mode that will be configured and activated by the L3 RRC procedure.

Setting

Range:

  • DTX (UL DTX)
  • DTRX (UL DTX + DL DRX)
  • HLESs (HS-SCCH-less)
  • DTHLess (UL DTX + HS-SCCH-less)
  • DTRHless (UL DTX + DL DRX + HS-SCCH-less)

Query

Range: DTX|DTRX|HLES|DTHL|DTRH

*RST Setting DTX
Requirements

Lab Application Revision: F.00.19 and above

Lab Application Revision F.01 and above, added HLESs, DTHLess, and DTRHless

Programming Example

 
OUTPUT 714;"CALL:CPC:MODE DTX"

CALL:CPC:MS:DPCChannel:BURSt[1]|2

Function

Sets/queries the UE DPCCH for the specified burst.

This parameter defines the length of the UL DPCCH transmission when UE DTX cycle 1 or UE DTX cycle 2 is active in the subframe unit.

Setting

Range: SUBFrames1|SUBFrames2|SUBFrames5

Query

Range: SUBF1|SUBF2|SUBF5

*RST Setting SUBFrames1
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MS:DPCChannel:BURSt2 SUBFrames1"
!Sets the length of the UL DPCCH transmission to 1 subframe for UE DTX cycle 2.

CALL:CPC:MS:DRX:CYCLe

Function

Sets/queries the UE DRX Cycle.

This parameter defines the HS-SCCH reception pattern when running the DL DRX operation after an inactive period of HS-SCCH reception defined by the "Inactivity Threshold for UE DRX Cycle" parameter. This specifies how often the UE has to monitor one HS-SCCH subframe of its HSSCCH set.

Setting

Range: SUBFrames4|SUBFrames5|SUBFrames8|SUBFrames10|SUBFrames16|SUBFrames20

Query

Range: SUBF4|SUBF5|SUBF8|SUBF10|SUBF16|SUBF20

*RST Setting SUBFrames10
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MS:DRX:CYCLe SUBFrames10"

CALL:CPC:MS:DRX:CYCLe:ITHReshold

Function

Sets/queries the Inactivity Threshold for UE DRX Cycle.

When running a DL DRX operation, this parameter defines a time period in subframe units after the last HS-SCCH reception that was not a HS-SCCH order where the UE has to continuously monitor the HS-SCCH.

Setting

Range: SUBFrames0|SUBFrames1|SUBFrames2|SUBFrames4|SUBFrames8|SUBFrames16|SUBFrames32|SUBFrames64|SUBFrames128|SUBFrames256|SUBFrames512

Query

Range: SUBF0|SUBF1|SUBF2|SUBF4|SUBF8|SUBF16|SUBF32|SUBF64|SUBF128|SUBF256|SUBF512

*RST Setting SUBFrames32
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MS:DRX:CYCLe:ITHReshold SUBFrames32"

CALL:CPC:MS:DRX:GMONitoring

Function

Sets/queries the UE DRX Grant Monitoring.

When running the DL DRX operation, this parameter controls whether the UE is required to monitor E-AGCH/E-RGCH from serving E-DCH cell when they overlap with the start of an HS-SCCH reception as defined in the HS-SCCH reception pattern using the "UE DRX Cycle" parameter.

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (On)

Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MS:DRX:GMONitoring ON"
! Sets UE DRX Grant Monitoring to On.

CALL:CPC:MS:DTX:CYCLe1[:MS10]

Function

Sets/queries the UE DTX Cycle 1 (10ms TTI).

This parameter is a part of the UL DPCCH burst pattern definition for UL DTX operation that defines how often the UE has to transmit UL DPCCH slots when UE DTX cycle 1 is active for the 10 ms E-DCH TTI.

Setting

Range: SUBFrames1|SUBFrames5|SUBFrames10|SUBFrames20

Query

Range: SUBF1|SUBF5|SUBF10|SUBF20

*RST Setting SUBFrames10
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CCALL:CPC:MS:DTX:CYCLe1 SUBFrames10"

CALL:CPC:MS:DTX:CYCLe1:MS2

Function

Sets/queries the UE DTX Cycle 1 (2ms TTI).

This parameter is a part of the UL DPCCH burst pattern definition for UL DTX operation that defines how often the UE has to transmit UL DPCCH slots when UE DTX cycle 1 is active for 2 ms E-DCH TTI.

Setting

Range: SUBFrames1|SUBFrames4|SUBFrames5|SUBFrames8|SUBFrames10|SUBFrames16|SUBFrames20

Query

Range: SUBF1|SUBF4|SUBF5|SUBF8|SUBF10|SUBF16|SUBF20

*RST Setting SUBFrames8
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MS:DTX:CYCLe1:MS2 SUBFrames8"

CALL:CPC:MS:DTX:CYCLe2:ITHReshold

Function

Sets/queries the Inactivity Threshold for UE DTX Cycle 2.

This parameter defines how long the UE will wait to transit from UE DTX cycle 1 to UE DTX cycle 2 after the last E-DCH transmission when running the UL DTX. This time period is in E-DCH TTI units based on the value of the HSUPA TTI Mode parameter.

Setting

Range: ETTis1|ETTis4|ETTis8|ETTis16|ETTis32|ETTis64|ETTis128|ETTis256

Query

Range: ETT1|ETT4|ETT8|ETT16|ETT32|ETT64|ETT128|ETT256
*RST Setting ETTis8
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MS:DTX:CYCLe2:ITHReshold ETTis8"

CALL:CPC:MS:DTX:CYCLe2[:MS10]

Function

Sets/queries the UE DTX Cycle 2 (10ms TTI).

This parameter is a part of UL DPCCH burst pattern definition for UL DTX operation that defines how often the UE has to transmit UL DPCCH slots when UE DTX cycle 2 is active for 10ms E-DCH TTI.

Setting

Range: SUBFrames5|SUBFrames10|SUBFrames20|SUBFrames40|SUBFrames80|SUBFrames160

Query

Range: SUBF5|SUBF10|SUBF20|SUBF40|SUBF80|SUBF160
*RST Setting SUBFrames20
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MS:DTX:CYCLe2[:MS10] SUBFrames20"

CALL:CPC:MS:DTX:CYCLe2:MS2

Function

Sets/queries the AMR Rate for SRB5 12.2k to 4.75k RAB.

Setting

Range: SUBFrames4|SUBFrames5|SUBFrames8|SUBFrames10|SUBFrames16|SUBFrames20 | SUBFrames32|SUBFrames40|SUBFrames64|SUBFrames80|SUBFrames128|SUBFrames160

Query

Range: SUBF4|SUBF5|SUBF8|SUBF10|SUBF16|SUBF20|SUBF32|SUBF40|SUBF64|SUBF80|SUBF128|SUBF160

*RST Setting SUBFrames16
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MS:DTX:CYCLe2:MS2 SUBFrames16"

CALL:CPC:MS:DTX:LPLength

Function

Sets/queries the UE DTX Long Preamble Length.

This parameter defines the long preamble length in slots that the UE uses when running UL DTX cycle 2 to aid synchronization.

Setting

Range: SLOTs4|SLOTs15

Query

Range: SLOT4|SLOT15

*RST Setting SLOTs4
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MS:DTX:LPLength SLOTs4"

CALL:CPC:MS:DTX:LPLength:INFormation[:STATe]

Function

Sets/queries the UE DTX Long Preamble Length Information State.

This setting controls whether the UE DTX long preamble length IE is signalled to the UE in an OTA RRC message when starting or reconfiguring a UL DTX operation:

  • When set to Off, the UE DTX long preamble length IE will be absent from a given RRC message to start or reconfigure the UL DTX operation. The UE will use '2 slots' as the DTX long preamble length default.
  • When set to On, the UE DTX long preamble length IE will be present, and the value for this parameter is defined using the "UE DTX Long Preamble Length" parameter.

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (On)

Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MS:DTX:LPLength:INFormation ON"
! Sets UE DTX Long Preamble Length Information State to On.

CALL:CPC:MS:GMONitoring:ITHReshold

Function

Sets/queries the Inactivity Threshold for UE Grant Monitoring.

When running the DL DRX this setting is used to configure a duration in E-DCH TTI units after an immediate scheduled E-DCH transmission in the UL where the UE has to listen to the E-AGCH from the serving E-DCH cell and the E-RGCH from all the cells in the E-DCH active cell.

Setting

Range: ETTis0|ETTis1|ETTis2|ETTis4|ETTis8|ETTis16|ETTis32|ETTis64|ETTis128|ETTis256

Query

Range: ETT0|ETT1|ETT2|ETT4|ETT8|ETT16|ETT32|ETT64|ETT128|ETT256

*RST Setting ETTis8
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MS:GMONitoring:ITHReshold AMR1220 ETTis8"

CALL:CPC:MS:OFFSet

Function

Sets/queries the UE DTX DRX Offset.

This parameter is common for UL DTX and DL DRX operation and defines a UE specific offset in subframe units for the UL DPCCH transmission pattern and DL HSSCCH reception pattern.

Setting

Range: 0 to 159

Query

Same as setting
*RST Setting 0
Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:MS:OFFSet 0"

CALL:CPC:STATe

Function

Sets/queries the CPC State.

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (Off)

Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:CPC:STATe OFF"
! Sets CPC State to Off.