CALL:DPCHannel

CALL:DPCHannel

Last updated: November 12, 2010

GPIB Command Conventions

CALL:DPCHannel[:SLEVel]

Function

Sets/queries the dedicated physical channel's (DPCH) initial downlink offset, and sets its state to ON.

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range: -30.00 dB to 0 dB (Prior to A.03, the range is -20.00 dB to 0 dB)

Resolution: 0.01

Query

Range: -30.00 dB to 0 dB (Prior to A.03, the range is -20.00 dB to 0 dB)

Resolution: 0.01

*RST Setting

-12.00 dB (off)

Requirements

Test Application Revision: A.03 and above

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:SLEVEL -12" 

CALL[:CELL]:DPCHannel:ASET:ADD:AUX

Function

Performs an Add DPCH (Aux Node) to Active Set event.

The purpose of this event is to create a DPCH on the Aux node and signal to the UE to add it to the active set. This event is only valid when Multi-Cell UTRAN mode is active and a call is active on the Main node but no DPCH is currently assigned on the Aux node.If the operation is successful, the Multi-Cell UTRAN Status of the Aux node will change from "Aux" to "A-Act" to indicate dedicated channels are now assigned.

Requirements

Lab Application Revision: F.01 and above.

Programming Example

 
OUTPUT 714;"CALL:DPCHannel:ASET:ADD:AUX"

CALL[:CELL]:DPCHannel:ASET:ADD:MAIN

Function

Performs an Add DPCH (Main Node) to Active Setevent.

The purpose of this event is to create a DPCH on the main node and signal to the UE to add it to the active set. This event is only valid when Multi-Cell UTRAN mode is active and a call is active on an Aux node but no DPCH is currently assigned from the Main node.If the operation is successful, the Multi-Cell UTRAN Status of the main node will change from "M-Ext" to "M-SHO" to indicate dedicated channels are now assigned on both nodes

Requirements

Lab Application Revision: F.01 and above.

Programming Example

 
OUTPUT 714;"CALL:DPCHannel:ASET:ADD:MAIN"

CALL[:CELL]:DPCHannel:ASET:REMove:AUX

Function

Performs a Remove DPCH (Aux Node) from Active Set event.

The purpose of this event is to release the DPCH on the Aux node and signal to the UE to remove it from the active set. This event is only valid when Multi-Cell UTRAN mode is enabled and a call is active in which a DPCH from both the Main node and Aux node is present in the active set .If the operation is successful, the Aux node DPCH will be released and the Multi-Cell UTRAN Status will change from "A-Act" to "Aux". Meanwhile the status on the Main node will change to "M-Loc" indicating channels are only active on the Main node.

Requirements

Lab Application Revision: F.01 and above.

Programming Example

 
OUTPUT 714;"CALL:DPCHannel:ASET:REMove:AUX"

CALL[:CELL]:DPCHannel:ASET:REMove:MAIN

Function

Performs an Remove DPCH (Main Node) from Active Set event.

The purpose of this event is to release the DPCH on the main node and signal to the UE to remove it from the active set. This event is only valid when Multi-Cell UTRAN mode is enabled and a call is active in which a DPCH from both the Main node and Aux node is present in the active set.

If the operation is successful, the Main node DPCH will be released and the Multi-Cell UTRAN Status will change from "M-SHO" to "M-Ext". Meanwhile the status on the Aux node will remain at "A-Act" indicating channels are still active on the Aux node.

Requirements

Lab Application Revision: F.01 and above.

Programming Example

 
OUTPUT 714;"CALL:DPCHannel:ASET:REMove:MAIN"

CALL:DPCHannel:DOFFset

Function

Sets/queries Default DPCH Offset (DOFF) .

This setting cannot be changed when the data/call status is not idle.

Setting

Range: 0 to 75

Resolution: 1

Query Same as setting

*RST Setting

0 (0 x 512 chips)

Requirements

Test Application Revision: A.08.20 and above
Lab Application Revision: C.03 and above
Test Application Revision: A.17.00 and above, extend the range from 5 to 75
Lab Application Revision: G.01.00 and above, extend the range from 5 to 75

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:DOFFset 3"
! Sets Default DPCH Offset (DOFF) to 3 x 512 chips.

CALL:DPCHannel:KSPS15[:CCODe]

Function

THIS COMMAND IS OBSOLETE. Please use CALL:DPCHannel:KSPS15[:CCODe]:CODE .

Sets/queries the channelization code for the downlink DPCH with a physical data rate of 15 ksps.

Setting

Range: CODE12|CODE13|CODE20|CODE21|CODE40|CODE43|CODE58
|CODE126|CODE127|CODE142|CODE153|CODE174|CODE235|CODE255

Query

Same as setting

*RST Setting

CODE12

Requirements

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:KSPS15:CCODE CODE13"

CALL:DPCHannel:KSPS15[:CCODe]:CODE

Function

Sets/queries the channelization code for the downlink DPCH with a physical data rate of 15 ksps. Codes 0 and 1 are reserved for the CPICH and SCH/PCCPCH respectively.

See Downlink Channel Codes .

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range: 2 to 255

Resolution: 1

Query

Same as setting

*RST Setting

12

Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:KSPS15:CODE 12"

CALL:DPCHannel:KSPS15[:CCODe]:CODE:HSDPa

Function

Sets/queries the HSDPA/HSPA DPCH 15 ksps (OVSF 256) Channelization Code.

See Downlink Channel Codes .

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range: 2 to 255

Resolution: 1

Query

Same as setting

*RST Setting

40

Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above, with the required feature license

Programming Example

 
OUTPUT 714;"CALL:DPCHannel:KSPS15:CODE:HSDPa 40"

CALL:DPCHannel:KSPS15[:CCODe]:HSDPa

Function

THIS COMMAND IS OBSOLETE. Please use CALL:DPCHannel:KSPS15[:CCODe]:CODE:HSDPa .

Sets/queries the HSDPA/HSPA DPCH 15 ksps (OVSF 256) Channelization Code.

Setting

Range: CODE40|CODE43|CODE58

Query

Same as setting

*RST Setting

CODE40

Requirements

Lab Application Revision: D.00 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHannel:KSPS15:HSDPa CODE43"

CALL:DPCHannel:KSPS30[:CCODe]

Function

THIS COMMAND IS OBSOLETE. Please use CALL:DPCHannel:KSPS30[:CCODe]:CODE .

Sets/queries the channelization code for the downlink DPCH with a physical data rate of 30 ksps.

Setting

Range: CODE6|CODE9|CODE10|CODE20|CODE29|CODE37|CODE45
|CODE54|CODE60|CODE63|CODE70|CODE76|CODE87|CODE93
|CODE112|CODE118

Query

Same as setting

*RST Setting

CODE9

Requirements

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:KSPS30:CCODE CODE10"

CALL:DPCHannel:KSPS30[:CCODe]:CODE

Function

Sets/queries the channelization code for the downlink DPCH with a physical data rate of 30 ksps.

See Downlink Channel Codes .

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range: 1 to 127

Resolution: 1

Query

Same as setting

*RST Setting

9

Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:KSPS30:CODE 9"

CALL:DPCHannel:KSPS30[:CCODe]:CODE:HSDPa

Function

Sets/queries the HSDPA/HSPA DPCH 30 ksps (OVSF 128) Channelization Code.

See Downlink Channel Codes .

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use cell off operating mode when changing this value.

Setting

Range: 1 to 127

Query

Same as setting

*RST Setting

20

Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above, with the required feature license

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:KSPS30:CODE:HSDPa 20"

CALL:DPCHannel:KSPS30[:CCODe]:HSDPa

Function

THIS COMMAND IS OBSOLETE. Please use CALL:DPCHannel:KSPS30[:CCODe]:HSDPa .

Sets/queries the HSDPA/HSPA DPCH 30 ksps (OVSF 128) Channelization Code.

Setting

Range: CODE20|CODE29|CODE37|CODE45|CODE54

Query

Same as setting

*RST Setting

CODE20

Requirements

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:KSPS30:HSDPa CODE29"

CALL:DPCHannel:KSPS60[:CCODe]:CODE

Function

Sets/queries the channelization code for the downlink DPCH with a physical data rate of 60 ksps.

See Downlink Channel Codes .

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range: 1 to 63

Resolution: 1

Query

Same as setting

*RST Setting

54

Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHannel:KSPS60:CODE 54"

CALL:DPCHannel:KSPS120[:CCODe]

Function

THIS COMMAND IS OBSOLETE. Please use CALL:DPCHannel:KSPS120[:CCODe]:CODE .

Sets/queries the channelization code for the downlink DPCH with a physical data rate of 120 ksps.

Setting

Range: CODE6|CODE10|CODE12|CODE14|CODE16|CODE18
|CODE20|CODE22|CODE24|CODE25|CODE26|CODE27

Query

Same as setting

*RST Setting

CODE6

Requirements

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:KSPS120 CODE10"

CALL:DPCHannel:KSPS120[:CCODe]:CODE

Function

Sets/queries the channelization code for the downlink DPCH with a physical data rate of 120 ksps.

See Downlink Channel Codes .

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range:1 to 31

Resolution: 1

Query

Same as setting

*RST Setting

6

Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHannel:KSPS120:CODE 6"

CALL:DPCHannel:KSPS240[:CCODe]

Function

THIS COMMAND IS OBSOLETE. Please use CALL:DPCHannel:KSPS240[:CCODe]:CODE .

Sets/queries the channelization code for the downlink DPCH with a physical data rate of 240 ksps.

Setting

Range: CODE12|CODE13

Query

Same as setting

*RST Setting

CODE12

Requirements

Lab Application Revision: B.01 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:KSPS240:CCODE CODE13"
! Sets the 240 ksps channelization code to 13.

CALL:DPCHannel:KSPS240[:CCODe]:CODE

Function

Sets/queries the channelization code for the downlink DPCH with a physical data rate of 240 ksps.

See Downlink Channel Codes .

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range:1 to 15

Resolution: 1

Query

Same as setting

*RST Setting

12

Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHannel:KSPS240:CODE 12"

CALL:DPCHannel:KSPS480[:CCODe]

Function

THIS COMMAND IS OBSOLETE. Please use CALL:DPCHannel:KSPS480[:CCODe]:CODE .

Sets/queries the channelization code for the downlink DPCH with a physical data rate of 480 ksps.

Setting

Range: CODE6

Query

Same as setting

*RST Setting

CODE6

Requirements

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:KSPS480:CCODE CODE6"

CALL:DPCHannel:KSPS480[:CCODe]:CODE

Function

Sets/queries the channelization code for the downlink DPCH with a physical data rate of 480 ksps.

See Downlink Channel Codes .

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range:6

Query

Same as setting

*RST Setting

6

Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHannel:KSPS480:CODE 6"

CALL:DPCHannel:LEVel

Function

Sets/queries the dedicated physical channel's (DPCH) initial downlink offset.

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range: -30.00 dB to 0 dB (Prior to A.03, the range is -20.00 dB to 0 dB)

Resolution: 0.01

Query

Range: -30.00 dB to 0 dB (Prior to A.03, the range is -20.00 dB to 0 dB)

Resolution: 0.01

*RST Setting

-12.00 dB

Requirements

Test Application Revision: A.03 and above

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:LEVEL -12" 

CALL:DPCHannel:RMC12:CCODe

Function

Sets/queries the dedicated physical control channel's channelization code for the 12.2 kbps reference measurement channel, the 12.2k AMR Voice channel, 33k No Coding RMC and 13.6k DCCH (SRB). See Downlink Channel Codes .

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range: CODE6|CODE9|CODE10|CODE20|CODE29|CODE37|CODE45
|CODE54|CODE60|CODE63|CODE70|CODE76|CODE87|CODE93
|CODE112|CODE118

Query

Range: CODE6|CODE9|CODE10|CODE20|CODE29|CODE37|CODE45
|CODE54|CODE60|CODE63|CODE70|CODE76|CODE87|CODE93
|CODE112|CODE118

*RST Setting

CODE9

Requirements

Test Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:RMC12:CCODE CODE6"
! Sets the 12.2 RMC's channelization code.

CALL:DPCHannel:RMC12:CCODe:HSDPa

Function

Sets/queries the HSDPA/HSPA DPCH 12.2k RMC Channelization Code. See Downlink Channel Codes and HSDPA in FDD Test Operating Mode .

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range: CODE20|CODE29|CODE37|CODE45|CODE54

Query

Same as setting

*RST Setting

CODE20

Requirements

Test Application Revision: A.08 and above, with the required feature license

Lab Application Revision: C.03 and above.

Programming Example

 
OUTPUT 714;"CALL:DPCHannel:RMC12:CCODe:HSDPa CODE29"
! Sets the HSDPA DPCH 12.2k RMC channelization code.

CALL:DPCHannel:RMC64:CCODe

Function

Sets/queries the dedicated physical control channel's 64 kbps reference measurement channel's channelization code.

The type of bearer service being carried by the WCDMA link drives the configuration of the DTCH and DCCH logical channels, the DCH Transport channel, and the DPCH physical channel. The test set supports only symmetrical channels, and only one type of bearer service at a time.

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range: CODE6|CODE10|CODE12|CODE14|CODE16|CODE18
|CODE20|CODE22|CODE24|CODE25|CODE26|CODE27

Query

Same as setting

*RST Setting

CODE6

Requirements

Test Application Revision: A.02 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:RMC64:CCODE CODE10"
! Sets the 64 RMC's channelization code.

CALL:DPCHannel:RMC144:CCODe

Function

Sets/queries the DPCH 144k RMC Channelization Code (see Downlink Channel Codes ).

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range: CODE12|CODE13

Query

Same as setting

*RST Setting

CODE12

Requirements

Test Application Revision: A.05 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:RMC144:CCODE CODE13"
! Sets the 144k RMC's channelization code to 13.

CALL:DPCHannel:RMC384:CCODe

Function

Sets/queries the dedicated physical control channel's 384 kbps reference measurement channel's channelization code.

The type of bearer service being carried by the WCDMA link drives the configuration of the DTCH and DCCH logical channels, the DCH Transport channel, and the DPCH physical channel. The test set supports only symmetrical channels, and only one type of bearer service at a time.

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range: CODE6

Query

Same as setting

*RST Setting

CODE6

Requirements

Test Application Revision: A.04 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:RMC384:CCODE CODE6"
! Sets the 384k RMC's channelization code.

CALL:DPCHannel:STATe

Function

Sets/queries the dedicated physical control channel's state.

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range: 1|ON | 0|OFF

Query

Range: 1|ON | 0|OFF

*RST Setting

0 (off)

Requirements

Test or Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:STAT 1" 

CALL:DPCHannel:TYPe

Function

THIS COMMAND IS OBSOLETE. Please use the CALL:SERVice:RBTest:RAB command to set/query channel type.

Sets/queries the dedicated physical control channel's channel type. See Channel Type .

This setting cannot be changed while in active cell operating mode. Attempting to change this setting while in this mode results in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this value.

Setting

Range:

  • RMC12
  • RMC64
  • RMC384

Query

Same as setting.

*RST Setting

RMC12

Requirements

Test Application Revision: A.01 and above

Test Application Revision A.02 added RMC64

Test Application Revision A.04 added RMC384

Lab Application Revision: A.01 and above.

Lab Application Revision A.02 added RMC384

Programming Example

 
OUTPUT 714;"CALL:DPCHANNEL:TYPE RMC12"
! Selects the 12.2 RMC for the DPCH.