CALL:MS:REPorted

CALL:MS:REPorted

Last updated: April 27, 2013

GPIB Command Conventions

CALL:MS:REPorted:AUTHenticate:FAILcause?

Function

Queries the UE Reported Failure Cause .

Query

Range: 1 to 255, 9.91E +37

*RST Setting

9.91E +37

Requirements

Test Application Revision: A.03 and above.

Lab Application Revision: A.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:AUTHenticate:FAILcause?"
!Queries the authentication fail cause.

CALL:MS:REPorted:CAPability:DCHSdpa:DBANd?

Function

Queries the Configuration 1/2/3/4/5 Supported by UE .

Query

Range: 16 elements with each element raning from 0....1.

Each element reflects a DB-DC-HSDPA configuration.

3GPP TS 25.331defines that there are 16 configurations at most. In 3GPP Release 9, there are three configurations defined in total, and there are two additional configurations added in 3GPP Release 10, thus only the first five elements make sense in these 16 elements. The X th element with the value 0 means the configuration on X is not supported by the UE, yet the value 1 means the configuration X is supported by the UE.

*RST Setting

0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0
Requirements

Test Application Revision: A.20.00 and above, with the required feature licence

Lab Application Revision: I.00.00 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:CAPability:DCHSdpa:DBANd?"
!Queries the DB-DC-HSDPA configuration(s) supported by the UE.

CALL:MS:REPorted[:CELL[1]]:ALL?

Function

Queries the UE (mobile station) reported measurement results after a successful Measurement Request (see CALL:MS:REPorted:MEASurement:REQuest ). The measurement results returned include CPICH Ec/No, Pathloss and CPICH RSCP (see UE Reported Measurements for more descriptions).

After a successful Measurement Request, three comma separated results are returned in the order of CPICH Ec/No, Pathloss, and CPICH RSCP. See CALL:MS:REPorted[:CELL[1]]:CPICh:ECNO? , CALL:MS:REPorted[:CELL[1]]:PATHloss? , and CALL:MS:REPorted[:CELL[1]]:CPICh:RSCP? for more information.

To obtain DTCH BLER results, see CALL:MS:REPorted[:CELL[1]]:DTCH:BLER? .

Query

CPICH Ec/No:

  • Range: 0 to 49, 9.91E +37

Pathloss:

  • Range: 46 to 158 dB, 9.91E +37
  • Resolution: 1 dB

CPICH RSCP:

  • Range: 0 to 91, 9.91E +37

*RST Setting

9.91E +37
Requirements

Test Application Revision: A.03 and above.

Lab Application Revision: A.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:ALL?"

CALL:MS:REPorted[:CELL[1]]:CPICh:ECNO?

Function

Queries the UE (mobile station) reported CPICH Ec/No measurement result which is an index to a range of Ec/No values. See CPICH Ec/No for the mapping of this report value to actual Ec/No range.

Query

Range: 0 to 49, or 9.91 E+37

*RST Setting

9.91E +37
Requirements

Test Application Revision: A.03 and above.

Lab Application Revision: A.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:CPICh:ECNO?"

CALL:MS:REPorted[:CELL[1]]:CPICh:RSCP?

Function

Queries the UE (mobile station) reported CPICH RSCP measurement result which is an index to a range of RSCP values. See CPICH RSCP (Received Signal Code Power) for the mapping of this report value to actual RSCP range.

Query

Range: -5 to 91, or 9.91 E+37

*RST Setting

9.91E +37
Requirements

Test Application Revision: A.03 and above.

Lab Application Revision: A.01 and above.

Lab Application Revision: I.01.00 and above, extended the range from 0 -- 91 to -5 -- 91.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:CPICh:RSCP?"

CALL:MS:REPorted[:CELL[1]]:PATHloss?

Function

Queries the UE (mobile station) reported Pathloss measurement result in the unit of dB. See Pathloss for more details.

Query

Range: 46 to 158 dB, or 9.91 E+37

Resolution: 1 dB

*RST Setting

9.91E +37
Requirements

Test Application Revision: A.03 and above.

Lab Application Revision: A.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:PATHloss?"

CALL:MS:REPorted[:CELL[1]]:DTCH:BLER?

Function

Queries the UE (mobile station) reported DTCH BLER measurement result which is an index to a range of BLER values. See DTCH BLER (Block Error Ratio) Report for the mapping of this report value to actual BLER range.

Query

Range: 0 to 63, or 9.91 E+37

*RST Setting

9.91E +37
Requirements

Test Application Revision: A.03 and above.

Lab Application Revision: A.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:DTCH:BLER?"

CALL:MS:REPorted:CELL2:ALL?

Function

Queries the cell 2 UE (mobile station) reported measurement results after a successful Measurement Request (see CALL:MS:REPorted:MEASurement:REQuest ). The supported measurements include CPICH Ec/No, Pathloss and CPICH RSCP (see Cell 1/Cell 2 UE Reported Measurements for more information).

After a successful Measurement Request, three comma separated results are returned in the order of CPICH Ec/No, Pathloss, and CPICH RSCP. See CALL:MS:REPorted[:CELL[1]]:CPICh:ECNO? , CALL:MS:REPorted[:CELL[1]]:PATHloss? , and CALL:MS:REPorted[:CELL[1]]:CPICh:RSCP? for more information.

To obtain DTCH BLER results, see CALL:MS:REPorted[:CELL[1]]:DTCH:BLER? .

Query

CPICH Ec/No:

  • Range: 0 to 49, 9.91E +37

Pathloss:

  • Range: 46 to 158 dB, 9.91E +37
  • Resolution: 1 dB

CPICH RSCP:

  • Range: 0 to 91, 9.91E +37

*RST Setting

9.91E +37
Requirements Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:CELL2:ALL?"

CALL:MS:REPorted:CELL2:CPICh:ECNO?

Function

Queries the cell 2 UE (mobile station) reported CPICH Ec/No measurement result which is an index to a range of Ec/No values. See CPICH Ec/No for the mapping of this report value to actual Ec/No range.

Query

Range: 0 to 49, 9.91E +37

*RST Setting

9.91E +37
Requirements Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:CELL2:CPICh:ECNO?"

CALL:MS:REPorted:CELL2:CPICh:RSCP?

Function

Queries the cell 2 UE (mobile station) reported CPICH RSCP measurement result which is an index to a range of RSCP values. See CPICH RSCP (Received Signal Code Power) for the mapping of this report value to actual RSCP range.

Query

Range: -5 to 91, 9.91E +37

*RST Setting

9.91E +37
Requirements

Lab Application Revision: A.01 and above.

Lab Application Revision: I.01.00 and above, extended the range from 0 -- 91 to -5 -- 91.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:CELL2:CPICh:RSCP?"

CALL:MS:REPorted:CELL2:OTDifference[:VALue]?

Function

Queries the UE reported SFN-SFN Observed Time Difference (OTD) measurement result. The type of OTD measurement performed by the UE can be queried using the CALL:MS:REPorted:CELL2:OTDifference:TYPE? command.

Query

Range: 0 to 9830399 chips, 9.91E +37

Resolution: 1 chip

*RST Setting

9.91E +37
Requirements Lab Application Revision: C.01 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:CELL2:OTDifference?"

CALL:MS:REPorted:CELL2:OTDifference:TYPE?

Function

Queries the type of SFN-SFN Observed Time Difference (OTD) measurement performed by the UE. The UE reported OTD measurement result can be queried using the CALL:MS:REPorted:CELL2:OTDifference[:VALue]? command.

Query

Range: NONE|TYPE1|TYPE2

*RST Setting

NONE
Requirements Lab Application Revision: C.01 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:CELL2:OTDifference:TYPE?"

CALL:MS:REPorted:CELL2:PATHloss?

Function

Queries the cell 2 UE reported Pathloss measurement result.

Query

Range: 46 to 158 dB, 9.91E +37

Resolution: 1 dB

*RST Setting

9.91E +37
Requirements Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:CELL2:PATHloss?"

CALL:MS:REPorted:CLEar[:ALL]<[:SELected]|:WCDMa>

Function

Clears the UE (mobile) reported information. See Clear UE Info .
Requirements

Test Application Revision: A.04 and above

Lab Application Revision: A.02 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:CLEar"

CALL:MS:REPorted:CONText:SESSion:MAXimum?

Function

Queries the UE Reported Max Context Session.

This result is extracted from the "PDCP Capability" IE in the RRC Connection Setup Complete message. If the UE did not report this, NaN is returned. This value is used to determine the MAX_CID parameter for both uplink and downlink that will be used to configure the UE.

Query

Range: 1 to 16383, 9.91E +37

*RST Setting

9.91E +37

Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:CONText:SESSion:MAXimum?"
!Queries the UE Reported Max Context Session.

CALL:MS:REPorted:DOWNlink:RDDepth?

Function

Queries the UE Reported Downlink Reverse Decompression Depth.

This result is extracted from the "PDCP Capability" IE in the RRC Connection Setup Complete message. If the UE did not report this, NaN is returned.

Query

Range: 0 to 65535, 9.91E +37

*RST Setting

9.91E +37

Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"ALL:MS:REPorted:DOWNlink:RDDepth?"
!Queries the UE Reported Downlink Reverse Decompression Depth.

CALL:MS:REPorted:EISV?

Function

Queries the International Mobile station Equipment Identity and Software Version number (IMEISV) reported by the UE. This result is not available when CALL[:CELL]:EIDentity:REQuest] is set to "IMEI". The IMEISV is composed of the following elements:

- Type Allocation Code (TAC). Its length is 8 digits;- Serial Number (SNR) is an individual serial number uniquely identifying each equipment within each TAC. Its length is 6 digits;- Software Version Number (SVN) identifies the software version number of the mobile equipment. Its length is 2 digits.

Query

Range: 0 to FFFFFFFFFFFFFFFF (16 chars, '0'-'9', 'A'-'F' in each char), No Results Available

*RST Setting

No Results Available
Requirements

Lab Application Revision: E.00.34 and above.

Test Application Revision: A.13 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:EISV?"

CALL:MS:REPorted:EISV:SVN?

Function

Queries only the Software Version Number (SVN) element of the IMEISV reported by the UE. The SVN identifies the software version number of the mobile equipment. Its length is 2 digits.

This result is not available when CALL[:CELL]:EIDentity:REQuest] is set to "IMEI".

Query

Range: 0 to FF (2 chars, '0'-'9', 'A'-'F' in each char), No Results Available

*RST Setting

No Results Available
Requirements

Lab Application Revision: E.00.34 and above.

Test Application Revision: A.13 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:EISV:SVN?"

CALL:MS:REPorted:EUTRa:EARFcn?

Function

Queries the UE Reported EARFCN for E-UTRA Cells 1 to 8.

This result returns the first 8 cells that are present in the measurement report.

Query

Range: 0 to 65535

*RST Setting

No Results Available
Requirements Lab Application Revision: H.01.00 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:EUTRa:EARFcn?"

CALL:MS:REPorted:EUTRa:CID?

Function

Queries the UE Reported Cell ID for E-UTRA Cells 1 to 8.

This result is for the first 8 cells that are present in the measurement report.

Query

Range: 0 to 503
Requirements Lab Application Revision: H.01.00 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:EUTRa:CID?"

CALL:MS:REPorted:EUTRa:RSRP?

Function

Queries the UE Reported RSRP for E-UTRA Cells 1 to 8.

This result is for the first 8 cells that are present in the measurement report.

Query

Range: 0 to 97
Requirements Lab Application Revision: H.01.00 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:EUTRa:RSRP?"

CALL:MS:REPorted:EUTRa:RSRQ?

Function

Queries the UE Reported RSRQ for E-UTRA Cells 1 to 8.

This result is for the first 8 cells that are present in the measurement report.

Query

Range: 0 to 33
Requirements Lab Application Revision: H.01.00 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:EUTRa:RSRQ?"

CALL:MS:REPorted:EUTRa:CELLs?

Function

Queries the Total Number of E-UTRA Cells Reported by the UE.

This result returns the total number of E-UTRA cells that the UE included in its Measurement Result

Query

Range: 0 to 8
Requirements Lab Application Revision: H.01.00 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:EUTRa:CELLs?"

CALL:MS:REPorted:FREQuency[:SEParation]?

Function

Queries the "Band A" transmit/receive frequency separation. The specified frequencies are as follows: 190 MHz (MHZ190, fixed frequency separation), 174.8 to 205.2 MHz (MHZV205, variable frequency separation within this range), 134 to 245.2 MHz (MHZV245, variable frequency separation within this range).

Query

Range: MHZ190|MHZV205|MHZV245|NONE

*RST Setting

NONE
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:FREQuency?"

CALL:MS:REPorted:GSMSystem:BCHannel?

Function

Queries the BCH ARFCN result reported by the UE (for up to 8 GSM cells). Note that the cells are reported by the UE in order of RSSI strength. Use the CALL:MS:REPorted:GSMSystem:CIDentity? query to determine the Inter-RAT Cell ID for each of the reported cells.

Query

Range: 0 to 1023, 9.91E+37

Resolution: 1

*RST Setting

9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37
Requirements

Lab Application Revision: B.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:GSMSystem:BCHannel?"

CALL:MS:REPorted:GSMSystem:BSIC:VALue?

Function

Queries the BSIC Value corresponding to the Inter-RAT Cell ID reported by the UE (for up to 8 GSM cells). Note that the cells are reported by the UE in order of RSSI strength. Use the CALL:MS:REPorted:GSMSystem:CIDentity? query to determine the Inter-RAT Cell ID for each of the reported cells.

Query

Range: 0 to 77, 9.91E+37

*RST Setting

9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37
Requirements Lab Application Revision: D.00.04 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:GSMSystem:BSIC:VALue?"

CALL:MS:REPorted:GSMSystem:BSIC:VERification?

Function

Queries the BSIC Verification result reported by the UE (for up to 8 GSM cells). Note that the cells are reported by the UE in order of RSSI strength. Use the CALL:MS:REPorted:GSMSystem:CIDentity? query to determine the Inter-RAT Cell ID for each of the reported cells.

Query

Range:

  • VER - Verified
  • NVER - Not Verified
  • NREP - the cell was not measured by the UE

*RST Setting

NREP,NREP,NREP,NREP,NREP,NREP,NREP,NREP
Requirements Lab Application Revision: D.00.04 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:GSMSystem:BSIC:VERification?"

CALL:MS:REPorted:GSMSystem:CIDentity?

Function

GSM neighbor cells are reported by the UE in order of RSSI strength. This query returns the Inter-RAT Cell ID for each of the cells reported by the UE, to allow you to map the UE reported results to the SIB11 GSM cell info list neighbor cells.

Query

Range: 1 to 8, 9.91E+37

Resolution: 1

*RST Setting

9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37
Requirements Lab Application Revision: D.00.04 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:GSMSystem:CIDentity?"

CALL:MS:REPorted:GSMSystem:CELLs?

Function

Queries the UE reported Total Number of GSM Cells .

Query

Range: 0 to 8

Resolution: 1

*RST Setting

0
Requirements

Lab Application Revision: B.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:GSMSystem:CELLs?"

CALL:MS:REPorted:GSMSystem:RSSI?

Function

Queries the RSSI (GSM Cells) result reported by the UE (for up to 8 GSM cells). Note that the cells are reported by the UE in order of RSSI strength. Use the CALL:MS:REPorted:GSMSystem:CIDentity? query to determine the cell ID for each of the reported cells.

Query

Range: 0 to 63, 9.91E+37

Resolution: 1

*RST Setting

9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37
Requirements

Lab Application Revision: B.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:GSMSystem:RSSI?"

CALL:MS:REPorted:IMEI[:SELected]?

Function

Queries the mobile reported IMEI .

Query

Range: "0" to "FFFFFFFFFFFFFF" (0 to 15 characters from the set 0123456789ABCDEF) or "" (null string)

*RST Setting

"" (null string)

Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:IMEI?"

CALL:MS:REPorted:IMSI[:SELected]?

Function

Queries the mobile reported IMSI .

Query

Range: "0" to "FFFFFFFFFFFFFF" (0 to 15 characters from the set 0123456789ABCDEF) or "" (null string)

*RST Setting

"" (null string)
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:IMSI?"

CALL:MS:REPorted:ITRFrequency:CELLs?

Function

Queries the mobile reported total number of inter frequency cells (see Inter-Frequency Neighbor Cell Measurement Results ).

Query

Range: 0 to 32

Resolution: 1

*RST Setting

0
Requirements

Lab Application Revision: B.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:ITRFrequency:CELLs?"

CALL:MS:REPorted:ITRFrequency:DOWNlink:CHANnel?

Function

Queries the mobile reported DL channel for inter frequency cells 1-8 (see Inter-Frequency Neighbor Cell Measurement Results ).

Query

Range: 0 to 16383, 9.91E+37

Resolution: 1

*RST Setting

9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37
Requirements

Lab Application Revision: B.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:ITRFrequency:DOWNlink:CHANnel?"

CALL:MS:REPorted:ITRFrequency:ECNO?

Function

Queries the mobile reported Ec/No for inter frequency cells 1-8 (see Inter-Frequency Neighbor Cell Measurement Results ).

Query

Range: 0 to 49, 9.91E+37

Resolution: 1

*RST Setting

9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37
Requirements

Lab Application Revision: B.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:ITRFrequency:ECNO?"

CALL:MS:REPorted:ITRFrequency:PATHloss?

Function

Queries the mobile reported pathloss for inter frequency cells 1-8 (see Inter-Frequency Neighbor Cell Measurement Results ).

Query

Range: 46 to 158 dB, 9.91E+37

Resolution: 1 dB

*RST Setting

9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37
Requirements

Lab Application Revision: B.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:ITRFrequency:PATHloss?"

CALL:MS:REPorted:ITRFrequency:RSCP?

Function

Queries the mobile reported RSCP for inter frequency cells 1-8 (see Inter-Frequency Neighbor Cell Measurement Results ).

Query

Range: -5 to 91, 9.91E+37

Resolution: 1

*RST Setting

9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37
Requirements

Lab Application Revision: B.01 and above.

Lab Application Revision: I.01.00 and above, extended the range from 0 -- 91 to -5 -- 91.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:ITRFrequency:RSCP?"

CALL:MS:REPorted:ITRFrequency:RSSI?

Function

Queries the mobile reported RSSI for inter frequency cells 1-8 (see Inter-Frequency Neighbor Cell Measurement Results ).

Query

Range: 0 to 76, 9.91E+37

Resolution: 1

*RST Setting

9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37
Requirements

Lab Application Revision: B.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:ITRFrequency:RSSI?"

CALL:MS:REPorted:ITRFrequency:SCODe?

Function

Queries the mobile reported scrambling code for inter frequency cells 1-8 (see Inter-Frequency Neighbor Cell Measurement Results ).

Query

Range: 0 to 511, 9.91E+37

Resolution: 1

*RST Setting

9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37
Requirements

Lab Application Revision: B.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:ITRFrequency:SCODe?"

CALL:MS:REPorted:MEASurement:INTernal:STATe

Function

Sets/queries the UTRA FDD UE Internal Measurement State.

This setting controls whether the UE internal measurement is requested from the UE the next time that the Send Measurement Request action is invoked.

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (off)

Requirements

Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:MEASurement:INTernal:STATe 0"
! Sets UTRA FDD UE Internal Measurement State to off.

CALL:MS:REPorted:MEASurement:ITAFrequency:STATe

Function

Sets/queries UTRA FDD Intra-frequency Measurement State.

This setting controls whether the intra-frequency measurement is requested from the UE the next time that the Send Measurement Request action is invoked.

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)

Requirements

Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:MEASurement:ITAFrequency:STATe 1"
! Sets UTRA FDD Intra-frequency Measurement State to on.

CALL:MS:REPorted:MEASurement:OTDifference:TYPE

Function

Sets/queries the SFN-SFN OTD Measurement Type performed by the UE when the CALL:MS:REPorted:MEASurement:REQuest command is sent.

Setting Range: NONE|TYPE1|TYPE2
Query Same as setting.
*RST Setting NONE
Requirements

Lab Application Revision: C.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:MEASurement:OTDifference:TYPE TYPE2"
! Sets SFN-SFN OTD Measurement Type to Type 2.

CALL:MS:REPorted:MEASurement:QUALity:STATe

Function

Sets/queries UTRA FDD Quality Measurement State.

This setting controls whether the quality measurement is requested from the UE the next time that the Send Measurement Request action is invoked.

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (off)

Requirements

Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:MEASurement:QUALity:STATe 0"
! Sets UTRA FDD Quality Measurement State to off.

CALL:MS:REPorted:MEASurement:REQuest

Function

Sends a Measurement Control message, which orders the UE to perform measurements on cell 1 (and cell 2 if you are using the lab application). Which measurements are performed by the UE is determined by the CALL:MS:REPorted:MEASurement:TYPe and CALL:MS:REPorted:MEASurement:OTDifference:TYPE commands.
See Cell 1/Cell 2 UE Reported Measurements .

Requirements

Test Application Revision: A.03 and above.

Lab Application Revision: A.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:MEASurement:REQuest"

CALL:MS:REPorted:MEASurement:TYPe

Function

Sets/queries the Report Measurement Type , which determines which measurements are performed by the UE when the CALL:MS:REPorted:MEASurement:REQuest command is sent.
Setting

Range: ALL|INTRAFREQ|QUAL

Query

Same as setting.

*RST Setting

INTRAFREQ
Requirements

Test Application Revision: A.05 and above.

Lab Application Revision: B.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:MEASurement:TYPe ALL"

CALL:MS:REPorted:ONUMber<[:SELected]|WCDMa>?

Function

Queries the Called Party Number .

Query

Range: 0 to 20 characters enclosed by double quotes, from the set 0123456789.*# or "Emergency Call" or "" (null string).

*RST Setting

"" (null string)
Requirements

Lab Application Revision: C.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:ONUMber?"

CALL:MS:REPorted:PCLass[:SELected]?

Function

Queries the mobile reported Power Class .

Query

Range: 1, 2, 3, 4, 9.91E+37

*RST Setting

9.91E+37
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above.

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:PCLass?"

CALL:MS:REPorted:PRAChannel:SIGnature?

Function

Queries the Detected PRACH Signature .

Query

Range: 0 to 15, 9.91E+37

*RST Setting

9.91E+37

Requirements Lab Application Revision: A.02 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:PRAChannel:SIGnature?"

CALL:MS:REPorted:RINDicator?

Function

Queries the UE Reported Release Indicator.

During RRC Connection Setup procedure, the release 4 or later release UE can report the release number via message RRCConnectionRequest. UE can also report this indicator via message UECapabilityInformation.

Query

REL4 | REL5 | REL6 | REL7 | REL8 | 9.91E+37 (NAN)
Requirements Lab Application Revision H.01.00 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:RINDicator?"

CALL:MS:REPorted:TRANsmit:POWer?

Function

Queries the UTRA FDD UE Transmitted Power as an index.

The mapping of the reported value to actual UE transmission power range is provided in 3GPP TS 25.133 V7.d.0 section 9.1.6.2, "UE transmitted power measurement report mapping".

Query

Range: 0 to 104

Requirements Lab Application Revision: F.00.19 and above

Programming Example

 
OUTPUT 714;"CALL:MS:REPorted:TRANsmit:POWer?"
!Queries the the UTRA FDD UE Transmitted Power.