Queries the External 8960 Timing Measurement result.
This result is displayed on the Main node when Multi-Cell UTRAN mode is enabled successfully, or following the "Synchronize External 8960 Offset" event. It is defined as the number of frames and chips by which the external 8960s PCCPCH timing, leads the local 8960 and can be determined from the following equations.
Frames = ((((SFN_ext * 38400) + Chips_ext) - ((SFN_loc * 38400) + Chips_loc)) / 38400) % 4096Chips = ((((SFN_ext * 38400) + Chips_ext) - ((SFN_loc * 38400) + Chips_loc)) % 38400
|