Loopback Bit Error Ratio (BER) Measurement Description

Loopback Bit Error Ratio (BER) Measurement Description

Last updated: January 16, 2009

How Is a Loopback Bit Error Ratio Measurement Made?

3GPP TS 34.121, F.6.1.1 defines bit error ratio (BER) as follows: "The Bit Error Ratio is defined as the ratio of the bits wrongly received to all data bits sent. The bits are the information bits above the convolutional/turbo decoder."

When the test set measures loopback bit error ratio, it sends a known data pattern (see DL DTCH Data ) on the downlink dedicated traffic channel (DTCH) to a UE that is configured in loopback mode 1 or 2. (Although the measurement will operate with UE Loopback Type set to 2 , all TS 34.121 tests utilizing the BER measurement require loopback mode 1). The UE decodes the data and re-transmits it on the uplink DTCH. The test set analyzes the uplink data to see how closely it matches the data bits originally sent on the downlink. The test set compares the downlink and uplink data one transport block at a time and reports the Bit Error Ratio .

To decrease test time, you may set Confidence State to On and specify the BER Requirement , which allows the test set to stop testing when an early pass or early fail event occurs, and to report a Confidence Test Result (see 3GPP TS 34.121 F.6 and 3GPP TS 34.901).

3GPP TS 34.121 Figure F.6.1.9

Because the test set must compare the UE's uplink data with the corresponding downlink data, the measurement must be able to synchronize to the UE's signal (align received uplink transport blocks with their corresponding downlink transport blocks. In doing so, the test set determines the UE's Loopback Delay ). See Input Signal Requirements .

When testing the UE's receiver performance, it is assumed that the uplink is error free. Any errors occurring on the uplink invalidate the receiver test. The loopback BER measurement returns information about uplink CRC Errors to assist in ensuring that the uplink is error free (to perform the loopback BER measurement, you must set Uplink DTCH RMC CRC Presence to Present so that an uplink CRC is generated).

To perform the loopback BER measurement while in Active Cell Operating Mode , you must be on an RB test mode call, with Channel Type set to a symmetrical RMC. Loopback BER can not be measured for Asymmetrical RMCs .

The trigger source for this measurement is always protocol-based (see Trigger Source Description ).

UE Control During FDD Test Mode Operation

The FDD Test Operating Mode does not provide radio bearer setup control of the UE for test mode operation. You must configure the UE in loopback mode 1 or 2 and synchronize it to the test set's downlink signal in order to make this measurement in FDD test operating mode.

The uplink transport format must include both the DTCH and the DCCH; however, only the DTCH information is used for the loopback bit error ratio measurement.

Loopback BER Measurement Parameters

Loopback BER Measurement Results

Input Signal Requirements

Related Topics


Manual Operation: How Do I Make a Loopback Bit Error Ratio (BER) Measurement?

Programming a Loopback Bit Error Ratio Measurement

Loopback Bit Error Ratio Troubleshooting

Radio Bearer Test Mode and Channel Type

Block Error Ratio (BLER) Measurement Description

What 3GPP W-CDMA/HSPA Conformance Tests Are Supported?