Inner Loop Power Troubleshooting

Inner Loop Power Troubleshooting

Last updated: January 16, 2009

Possible Setup Issues

Interpreting Integrity Indicator Values

If Over Range (5) is returned, the measured signal exceeds the expected input level or exceeds the maximum allowed input power for the test set.

If Under Range (6) is returned, the measured signal is below the expected input level.

If Uncalibrated Due to Temperature (19) is returned, the temperature in the test set has changed by ± 10° C or more since the last calibration and should be calibrated again. Calibrating the Test Set .

Unable to Cal; Power unstable (24) is returned if, during test segments E-H, the UE does not properly respond to power control during the re-range periods.

See Integrity Indicator .

Related Topics