DUT IP Setup

DUT IP Setup

Last updated: April 27, 2013

This section is only applicable to the lab application.

Description

The test set supports three types of IP connection with the access terminal (AT, or also the Device Under Test): IPv4, IPv6 and IPv4+IPv6. Before the AT initiates an IP connection (either IPv4 or IPv6 or both) with the test set, the DUT IP parameters must be correctly set. A typical DUT IP Setup parameters menu is shown as below.

DUT IP Setup Menu

Related Topics


Packet Switched Data

Circuit Switched Data Service