E-UTRAN / WCDMA Interworking

E-UTRAN / WCDMA Interworking

Last updated: April 28, 2013

This section is only applicable to the lab application.

E-UTRAN / WCDMA Interworking Overview

E-UTRAN/WCDMA interworking relates to the test set working together with the Keysight E6621A PXT (See note below) to perform inter-Radio Access Technologies operations. This allows you to test the multi-mode wireless devices for LTE-WCDMA inter-RAT performance while using the test set as the WCDMA network simulator. In particular, the test set supports the following test scenarios:

For the hardware connection for these tests, see E-UTRAN / WCDMA Interworking Physical Connection .

For the inter-RAT frequency and priority information, see SIB19 Information .

   
NOTE
E-UTRAN / WCDMA interworking is restricted to using the Keysight E6621A PXT Wireless Communications Test Set as the LTE simulator. You must set up the PXT environment (cell configuration, RRC scenario, EPC, etc.) correctly so that the PXT emulates both the E-UTRAN and EPC functionalities for inter-RAT tests.

For detailed guidance on how to use the E6621A PXT, please refer to the E6621A user's guide at

http://cp.literature.keysight.com/litweb/pdf/E6621-90002.pdf


   

Before any LTE-WCDMA inter-RAT test, you must first set up a connection between the two simulators, for signaling and packet data transferring. Namely, you must set up the E-UTRAN / WCDMA Interworking Parameters and connect to the external LTE simulator successfully before performing any inter-RAT operations.

E-UTRAN / WCDMA Interworking Parameters

Manual Operation: You can access the following menu from the CALL SETUP hardkey, go to the left side Call Control 6 of 6 , then press the E-UTRAN/WCDMA Interworking Info ( F2 ).

E-UTRAN /WCDMA Interworking Information Screen

Evolved Packet Core (EPC) Connection Information

E-UTRAN / WCDMA Interworking Physical Connection

The figure below shows a typical Physical connection for E-UTRAN /WCDMA interworking.

  • Keysight PXT Test Set: working as the LTE system simulator whose functionalities and interfaces are in accordance with the standard.
  • Keysight 8960 Test Set: when running the E6703H lab application or above, the test set can work as a WCDMA network simulator.
  • Ethernet (LAN) Connection: interworking between the two systems relies on an ethernet connection to exchange signaling message or packet data.

    Note that there are two LAN Ports on the rear panel of the test set (See Rear Panel Connectors ). For E-UTRAN /WCDMA interworking, LAN 2 PORT is required to exchange signaling message or packet data. LAN 1 PORT is optional, but it is still useful for other LAN operations such as protocol logging, firmware downloads or screen captures.

  • RF Interface: The DUT must be able to communicate with both simulators. To accomplish this, it is common to use an RF splitter to connect the mobile to both test sets simultaneously.
  • GPIB Connection: GPIB connection between both test sets and a controlling PC are necessary if remote control of the instruments in the system is required.
  • Ethernet Switch or Hub: An ethernet switch or hub is needed in order for the Device Under Test to connect to external servers as well as for connecting the PC running WPA to the test sets.

Operating Considerations

  • Connecting to EPC requires the LAN 2 PORT to be configured and connected correctly. To set up the LAN 2 port on the front panel, press SYSTEM CONFIG hardkey and go to Control 1 of 2 , LAN IP Address 2 (Data+) setting is at the bottom of Instrument Setup (F1) menu.
  • Connecting/Disconnecting to the external EPC will cause any active PDP contexts to be deactivated.
  • The connection can be initiated from either the test set or the EPC simulator.
  • Ext EPC IP Addr must not be identical to the LAN IP Address setting. When the connection is successfully set up, Ext EPC IP Addr can not be changed.
  • On a full preset or format switch, the connection between the test set and the external EPC simulator will be interrupted.

Related Topics


GPIB Command: SYSTem:COMMunicate , SYSTem:STATus