Selecting the
trace format displays demodulated data using an IQ diagram (also called a polar or vector diagram). With an diagram, the VSA displays the in-phase signal (I) on the x-axis versus the quadrature-phase signal (Q) on the y-axis. The following information is provided:Each point represents a vector: the magnitude of the vector is determined by the distance from the origin to the IQ point and the phase is determined by the angle of the vector counterclockwise from the positive x-axis, as shown below.
Marker readouts show magnitude and phase or real and imaginary values. Markers hold their frequency (or time) position when changed between
and other trace formats (except constellation diagrams that do not include sub-symbol samples).To substitute real and imaginary values for magnitude and phase values in the marker readout, click Real & Imag for the Polar Format.
and selectFor
diagrams, the first marker readout is the magnitude, the next readout is the phase. If the marker's Polar Format is , the first marker readout is the x (or I) value, the next readout is the y (or Q) value.For ¾in this case, the IQ diagram would show 4 display points between each symbol.
diagrams in Digital Demod, the number of display points per symbol is determined by the value of . For example, if the value of is 1, each display point corresponds to a symbol. If the value is 5, the 5th display point corresponds to a symbolThe effect of Points / Symbol can be seen by displaying the diagram and pressing an arrow key or turning the mouse wheel to move the marker between symbols. If the number of points per symbol is 5, moving the marker would reveal four distinct display points between symbols.
The Constellation Diagrams topic for more information.
trace format behaves like the trace format, except that the format ignores the setting and only displays the samples at the symbol locations (similar to = 1). See the only applies toIn an Symbol Shape to dots or bars to highlight the symbols. Or toggle symbol to none to remove any highlighting.
diagram, the symbols (detection decision-points) can be highlighted or unhighlighted. SetThe number of symbols in the Result Length (Digital Demod) or the Measurement Interval (W-CDMA(3GPP)/cdma2000).
diagram is set by theThe colors used can be modified to represent symbols. To do this, click color-element and select the desired color.
, and click the tab. Then select the appropriate
To change this color: |
Modify these color elements: |
---|---|
Symbol color |
Symbol |
Annotation color | Trace |
Marker color | Selected Marker, Not Selected Marker |
Grid color | Grid |
See the Color Tab topic for more information.
Copyright © 2000-2023 Keysight Technologies, Inc. |