The Downlink Channel Properties dialog contains power boost and channel assignment controls for downlink frame transmission.
Power Boost - Sets the power boost level for each downlink physical channel or signals. NPDSCH power boost is separately controlled under Channel Configuration.
Subframe Channel Assignments - Assigns a downlink physical channel to each subframe by index (0:19). Some subframes have fixed channel assignments per the NB-IoT standard, as shown in the illustration below. The remaining subframes can be assigned either NPDCCH or NPDSCH.
See Also
Copyright © 2000-2023 Keysight Technologies, Inc. |