Using Standard Setups/Presets)
Selected (SeeIncludes pilot tracking in Error Vector Magnitude (EVM) calculations and adjusts constellation diagrams.
subcarrier constellation trace and then selecting and clearing the parameter. Similarly, display an EVM calculation, and then select and clear the parameter to see the effects of pilot error on the EVM calculation.
, when selected, causes the VSA to analyze the predicted locations of the pilot symbols on the sync/pilot locus versus the actual pilot symbol locations and add phase/amplitude corrections to better position the actual pilot symbols at the predicted locations. You can view this feature visually by displaying aSee Also
Copyright © 2000-2023 Keysight Technologies, Inc. |