Using Standard Setups/Presets)
1 (See.001 to 1000
Enter a
to scale the timebase of the signal you are using for measurement and analysis.The DAC (Digital to Analog Converter) clocking is scaled at a faster or slower rate. For example, you can scale a test signal with a symbol rate of 4Hz instead of 4000Hz by entering: Time Scale Factor = 0.001, which results in a correct analysis.
allows you to scale the timebase of a signal in a design or debug environment where the symbol rate andSee Also
Copyright © 2000-2023 Keysight Technologies, Inc. |