To perform a stimulus-response measurement with a single-channel instrument, you will need to measure the stimulus signal and save a trace of the signal's time data into a Data Register. Then you can measure the response signal from the DUT and compare the two signals.
Observe maximum input power limits. See the technical specifications for your measurement hardware to determine the maximum input limits.
Some Keysight signal generators provide user power limiting (e.g. to set a max input power level to your DUT). This is generally found in the
menu ("User Power Max" for the N5182A MXG).This procedure assumes you have configured an Keysight signal generator to provide the stimulus signal (perhaps by creating the signal in the Keysight Signal Studio software). If this describes your situation, you can skip to Initial Setup. If this is not exactly your situation, see the following paragraphs for variations on the procedure.
You can use something besides an Keysight signal generator as the stimulus; just be sure to provide a trigger signal from the stimulus source to the measurement hardware.
You can skip the Measure Stimulus section if you already have your stimulus signal recorded in a format that can be recalled by the VSA. Make sure the measurement hardware is being triggered when the beginning of the stimulus is sent into the DUT. In the case where you want to use an Keysight signal generator to send the stimulus signal, see the Use Keysight Signal Generator for Stimulus Signal topic.
Lastly, if your stimulus is inherently non-repeating, such as an AWGN signal, you can still perform a stimulus-response measurement by recording a section of the stimulus signal and using an Keysight signal generator to play the segment in a loop into your DUT. To do this, skip step 5f and use triggering instead when recording the stimulus (Measure Stimulus section). Then set triggering to after the Measure Stimulus section. You will also need to download the segment of the stimulus you recorded into your signal generator.
Connect the trigger output (for Keysight signal generators, use the EVENT 1 signal) of the source to the trigger input of the measurement instrument (make sure you use the primary trigger for your measurement hardware when there is more than one; for example, Trigger 1 IN).
Connect the 10 MHz OUT of the measurement instrument to the REF IN of the signal generator.
Connect the measurement instrument to your computer. See the Creating Hardware Configurations topic for more information.
Connect the signal generator to your computer. See the Creating Hardware Configurations topic for more information.
Configure the VSA
Preset the VSA (
). This will reset the VSA back to a basic Vector measurement.Select the Analyzer Configuration that contains your measurement hardware (from step 2)
Click
and choose from the list.Set the center frequency
Click
to open the dialog and then set the parameter.Set the
(also in the dialog)Span must be the same for both stimulus and response signals.
Set
Click the Choosing the Time Length for a discussion on choosing an appropriate time length.
tab in the MeasSetup dialog. SeeTo increase the range of the Main Time Length parameter, select the
check box.Configure triggering
Set triggering to External (click
and set to ).Connect the signal generator RF Output to the RF Input of your measurement instrument.
Run the measurement by clicking the Restart button in the toolbar and verify that your stimulus signal appears as expected.
Set the Range for your signal (
) or click the Auto-range button in the toolbar to ensure the best dynamic range for an accurate measurement.Save the stimulus signal
Click the
menu and select (Main Time).Click
Set
toSpecify a location to save the Main Time trace.
Click
Instead of saving the stimulus trace, you can copy the stimulus directly into a register (
) and then skip step 16 below.Connect the RF Output of the signal generator to the input of the device you are testing (DUT).
Connect the output of the DUT to the RF Input of the measurement instrument.
Switch to acquiring data from hardware by clicking
.Run the measurement by clicking the Restart button in the toolbar and verify that your response signal appears as expected.
Set the range for your signal (
) or click the Auto-range button in the toolbar to ensure the best dynamic range for an accurate measurement.Recall the stimulus data recording into data register D1
Click
and select the saved stimulus trace file. Click and then specify register when prompted.Add Graph traces
Add a new trace to the VSA (Click
)Select the type of Graph trace you want (Click ).
Initially, you might want to view AM/AM, AM/PM, and Gain Compression. Then, when you are trying to track down the cause of a high-EVM event, you might want to view the Delta EVM Time, Stimulus Time, and Response Time traces.
Configure Graph Settings (click )
You can skip steps i-iii. They are shown for your reference (the
selection should choose the correct data in this scenario).Clear the
check boxSet
toSet
toCustomize any of the other settings as desired
Autoscale the trace
When you don't see any data, the trace may be outside the limits of the trace grid. Try right-clicking in the center of the trace grid and choosing
.Repeat a-d to add more Graph traces if desired.
Instead of configuring each Graph trace in step c, you can configure one trace and skip step c for the other Graph traces. Once you are finished adding the Graph traces, select the configured trace and click
.Run the measurement
Click the Restart button in the toolbar.
See Also
Copyright © 2000-2023 Keysight Technologies, Inc. |