PCFICH is the Physical Control Format Indicator Channel and specifies how many OFDM symbols at the beginning of a subframe contain PDCCH. PCFICH is transmitted on the first OFDM symbol of a subframe and is transmitted only in subframes that contain symbols allocated to PDCCH.
The modulation type is QPSK.
See Section 6.7 of 3GPP TS 36.211 for more information about PCFICH.
See Also
Copyright © 2000-2023 Keysight Technologies, Inc. |