PDSCH is the Physical Downlink Shared Channel. This is the downlink data channel for users.
When RB Auto Detect is selected and RB Auto Detect Mode is set to , the demodulator groups resource blocks by modulation type and shows three groups ( , , and ) on the Frame Summary trace.
When RNTI.
is selected, and is set to , the demodulator decodes the allocations defined in the PDCCHs and shows each PDSCH allocation ( ) on the trace in increasing order ofWhen LTE Allocation Editor.
is cleared, shows a PDSCH allocation ( ) for each user mapping defined in theFor downlink signals, auto detection supports only PDSCH allocations transmitted on C-RS antenna ports.
A PDSCH allocation can contain a combination of QPSK, 16QAM, or 64QAM signals.
See Also
Copyright © 2000-2023 Keysight Technologies, Inc. |