MeasSetup Menu

The MeasSetup menu provides all the selections for setting up measurements.

This menu item…

Does this…

 

 

Frequency

Set up center and span or start and stop frequencies.

 

 

ResBW

Set up resolution bandwidth and data window parameters.

 

 

Time

Set up time and time gating parameters.

 

 

Detectors Select a detector for Power Spectrum measurements.
   
Conversion Set frequency conversion and image protection parameters for hardware used to make Power Spectrum measurements.
   

Average

Set up averaging parameters.

   
Frequency vs. Time Set up Frequency vs. Time analysis parameters.
   

Time vs. Time

Set up Time vs. Time analysis parameters.

   
New Measurement Add a new measurement of the specified type.
   
Duplicate Measurement Duplicate the specified measurement, including the measurement's selected hardware configuration and Shared status.
   
Remove Measurement Remove the specified measurement.
   

Measurements

Set up and control multiple measurements.

 

 

Measurement Type

Select the measurement type.

 

 

<meas type> Properties

Set up the selected measurement type and its associated parameters.