Selected (Measurements tab)

The Selected property is used to specify which particular measurement in a multi-measurement is the selected (or "active”) measurement. The selected measurement is indicated by a filled radio button in the Selected column and is the measurement that, by default, is modified by most other VSA controls and dialogs. Only one measurement may be selected (active).

The selected measurement also determines which other measurements are concurrently runnable; see Runnable Measurements.

In the Selected column, there is also a set of check boxes which determine which measurements are affected by the Multi-Measurement Controls Toolbar.

You can also use the measurement dropdown in the VSA main window toolbar to set the selected measurement.

See Also

Available Properties and Controls

Measurements Dialog