802.16 OFDM Standard Setups/Presets Table.
: SeeWhen OFDM burst and sets the VSAs demodulator to the modulation format specified in the text box. The modulation format is shown in the SubFrame Info trace data.
is selected, the Data Subcarrier Modulation Format can be manually specified. The VSA ignores the format transmitted in theFor more information, see Data Subcarrier Modulation topic
See Also
Format tab (IEEE 802.16 OFDM Demod Properties)
Copyright © 2000-2023 Keysight Technologies, Inc. |