The
tab of the dialog box configures the VSA's demodulator. These are the parameters necessary for the VSA to lock on to and demodulate the test signal.The
tab dialog box configures these parameters:See Also
IEEE 802.16 OFDM Demod Properties
Advanced Tab ( IEEE 802.16 OFDM Demod Properties)
Time Tab ( IEEE 802.16 OFDM Demod Properties)
Copyright © 2000-2023 Keysight Technologies, Inc. |