EVM for each subcarrier. The value displayed above each subcarrier index on the x-axis is the EVM RMS average for the subcarrier over all symbols in the Measurement Interval. Only currently selected channels (see Composite Include) are included in the average.
shows the Root Mean Square (RMS) averageThe value "ss" in the "xRMS: ss" or "xPeak: ss" annotation at the top of the trace is how many symbols were included in the current measurement.
This trace supports averaging over multiple measurements. When Averaging is enabled, value "mm" in the "RMS: mm" or "Peak: mm" annotation at the top of the trace displays how many measurement sweeps have been included in the current average.
See Also
Copyright © 2000-2023 Keysight Technologies, Inc. |