Last updated: November 7, 2012
This section is only applicable to the lab application.
SMS over SGs is an interim solution to realize the transmission of native SMS from CS infrastructure over the LTE radio network. Without SGs support, when a UE is camped on the LTE network, it would need to change its radio access technology back to 2G/3G, so as to process SMS service. SG is a new interface between the MME and the MSC. The SMS is transferred via SGs to MME and carried in NAS signaling to the UE, avoiding the need to execute fallback to a 2G/3G network.
The general procedure for a mobile terminated SMS is as follows:
The UE is camped on the LTE network, it is combined attached with EPS/IMSI, and updates MSC and MME with combined update procedure.
When the MSC receives an ingoing SMS, it will send a paging to the MME via SGs interface, then the MME will tunnel the paging message carried in NAS signaling to the UE.
The UE will respond to the paging message. Then the MSC will send the SMS via SGs interface towards the MME, which will tunnel the SMS carried in NAS signaling to the UE.
The figure below shows a typical Physical connection for SMS over SGs Test.
For detailed guidance on how to use the E6621A PXT, please refer to the E6621A user's guide at
http://cp.literature.keysight.com/litweb/pdf/E6621-90002.pdf
Note that there are two LAN Ports on the rear panel of the test set (See Rear Panel Connectors ). For E-UTRAN /GERAN interworking, LAN 2 PORT is required to exchange signaling message or packet data. LAN 1 PORT is optional, but it is still useful for other LAN operations such as protocol logging, firmware downloads or screen captures.
Before the test, you need to make the following operations:
At this point, the DUT is addressable on LTE. Should the DUT return to RRC idle it is necessary to first page the DUT to return it to RRC connected. Only when RRC connected can the following be executed.
Control 1 of 2
,
LAN IP Address 2(Data+)
setting is at the bottom of
Instrument Setup
(F1) menu.
Ext EPC IP Addr
must not be identical to the
LAN IP Address
setting. When the connection is successfully set up,
Ext EPC IP Addr
can not be changed.GPIB Command: SYSTem:COMMunicate , SYSTem:STATus , CALL:SMService:PTPoint[:MTERminated]:TRANsport