Source Setup Block Diagram

Instrument
AWG
DCA-X
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
NRZ
PAM4

The Configure Source for AWG dialog is used to configure many characteristics of the AWG waveform. These include amplitude, offset, and skew and the ability to add filtering, jitter, and interference. The capabilities shown in the dialog depend on whether the data source is data, clock, or imported in a waveform file.

You can click the channel button in this dialog to turn the AWG channel on and off.