Clipboard
Instrument
DCA-X
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Clipboard
In addition to the standard Windows keyboard shortcuts (Ctrl-C, Ctrl-X, Ctrl-V), you can drag and drop scalar measurements results and waveform widows to compatible Windows applications such as Microsoft Excel.

Use the copy-to-clipboard feature on FlexDCA's panel options flyout to place a screen shot into the Windows clipboard. You can then paste the screen shot into an application such as Microsoft Word. However, remember that this quick method does not save the screen image to a file for future use.