PAM Ceq
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
PAM4
The Eye mode PAM Ceq noise gain measurement measures the noise gain introduced by the following FlexDCA Waveform Signal Processing operators:
Although the Ceq measurement is defined by the standard for TDECQ measurements, it can be used with any of the operators that are listed above. Ceq is expressed as:
CeqdB = 10 log10(Noiseout / Noisein)