PAM Eye Heights
The fastest and recommended method of performing an Eye Height measurement on PAM4 waveforms is to use Jitter Mode's Eye Height measurement. Eye mode's Eye Height measurement can be used as a quick comparative check between signals. For example, when tuning pre-emphasis on a transmitter. In the following situations, you may want to use Eye Mode's measurement:
- For longer patterns, such as PRBS31Q, as Eye mode does not require pattern lock.
- When data is random or when measuring multiple waveforms at the same time.
The Eye mode PAM Eye Heights measurement measures the eye height (vertical opening) for each of three eyes of a PAM4 signal. On NRZ signals, the height of the single eye is measured. When the measurement is selected, the dialog shown here is displayed. All the settings in this dialog are linked to the settings in the PAM4 Eye Width dialog, except for the Select Signal field.
By default, the Select Measurement Source/Settings dialog has its Eye Opening Definition set to Zero Hits as shown in this picture. The eye opening is determined as the area in which there are no database hits.
Eye Opening Definition Set to "At Probability"
When the Eye Opening Definition is set to At Probability, the Select Measurement Source/Settings dialog appears as shown in this picture. The entered measurement-hit probability in the Eye Opening Probability field establishes the contour of an eye's opening.
Selecting Fix RJ or Fix RN turns on or off RJ and RN stabilization for PAM4 Eye Heights and Eye Widths measurements. To measure the value of RJ or RN to enter in this dialog, switch the 86100D to Jitter Mode and measure the RJ and RN while using a signal that has a short pattern. Or, measure the RN using a separate instrument. The Fix RJ or Fix RN settings that you enter for Eye Heights are also set for the Eye Widths measurement.

PAM-N Analysis Setup dialog Settings
To configure how the measurement is made, use the PAM-N Analysis Setup dialog box which provides the setting that are listed in the following table.
Setting | Description |
---|---|
Receiver Sample Timing | Configures the timing for sampling the signal data for all PAM measurements in Eye/Mask mode. |
Eye Center Location | Selects the basis for determining the location of an eye's center on the waveform. This can be set at the maximum eye width or maximum eye height. |
Eye Level Width | Defines the timespan (in percentage of symbol width) over which an eye's amplitude level is measured. |
Amplitude Units | Sets the amplitude units for measurement: volts, Watts, or percent. |
Measurement Algorithm
- An autoscale is performed to determine if the signal is formatted as PAM4 or NRZ.
- Determine the approximate signal-level amplitudes.
- Locate the crossing (transition) regions on both sides of the eyes.
- Determine the symbol period.
- Find the center of each eye. Note that the Receiver Sample Timing setting determines if only the middle eye (Eye 1/2) is located or if all three eyes are located (Eyes 0/1, 1/2, and 2/3).
- If the Eye Center Location setting is set to Maximum Eye Width, determine the horizontal line (center amplitude) across the eye at the maximum eye width and find the time at the line's midpoint (center time).
- If the Eye Center Location setting is set to Maximum Eye Height, determine the vertical line (center time) across the eye at the maximum eye height and find the amplitude at the line's midpoint (center amplitude).
- From the center of each eye the eye boundaries are located based on zero data "hits" or at an eye opening probability. The probability defines the ratio of total hits in a waveform database column that can occur in the eye's opening. The probablility can be set from 1 x 10–1 to 1 x 10–9 using the Eye Opening Probability setting. The default probability is 1 x 10–2. No extrapolation is used to determine Eye Widths at a specified probability.
- The Eye Height is reported.
To measure
- Select Eye/Mask Mode.
- Click Auto Scale in the menu toolbar.
- Click the toolbar's PAM tab.
- On the toolbar, locate and click the Eye Heights button.
SCPI Command
:MEASure:EYE:PAM:EHEight