Automatic Fixture Removal in TDR Mode

The Automatic Fixture Removal is a TDR Mode feature. This feature enables the Keysight N1930B Physical Layer Test System's Automatic Fixture Removal (AFR) de-embedding algorithm that has been directly ported into FlexDCA. The power of AFR is that it:

  • Characterizes the response of a fixture that has a non-connectorized port. Both single-ended and differential fixtures and probes can be characterized.
  • Saves an S-parameter Touchstone file (.s2p or .s4p) for importing into a TDR mode's Fixture Component. Fixture Components model the component to be de-embedded.