Legacy External Application Licenses

This topics covers legacy FlexDCA applications for which the licensing was handled by FlexDCA and shown in the FlexDCA Licensing dialog. These applications have been replaced by new application versions. These new applications:

  • Have new model numbers.
  • Do not appear in the FlexDCA Licensing dialog.
  • Are listed in the Keysight License Manager which is an application that is installed on the PC.
  • Do not return an identifier response string from the remote *OPT? query.
Legacy Application Licenses
Model Number Description *OPT?1
N1012A-CEI OIF CEI Compliance Application CEI
N1014A-1FP SFF-8431 Host Measurement Suite HST
N1014A-2FP SFF-8431 Module Measurement Suite MOD
N1019A-UDA User Defined Application MYC
N1081A-1FP IEEE 802.3ap/ba, Clauses 72,84 IE1
N1082A-1FP IEEE 802.3ba, Clauses 83A,83B,86A IE2
N1082A-4FP IEEE 802.3bm-2015 CAUI-4 Measurements CA4
N1083A-1FP IEEE 802.3ba, Clause 85 IE3
N1084A-1FP IEEE 802.3bj, Clauses 92,93 IE4
N1085A-1FP IEEE 802.3bs Draft PAM4 Measurements PM1
N1085A-4FP OIF-CEI 56G Draft PAM4 Measurements PM4
N1091BSCA IEEE 802.3bs/cd Measurement Application PM2
N109256CA OIF-CEI-56G-VSR/MR/LR Measurement Application PM5
N1091BSUA IEEE 802.3bs/cd Measurement Application, N1085A Upgrade PM2U
N109256UA OIF-CEI-56G-VSR/MR/LR Measurement Application, N1085A Upgrade PM5U
Footnotes:
1. Characters that identify a feature in the string returned by the *OPT? common programming query.
Legacy Switch Control Licenses
Description Model Number OPT?1
Advanced Eye Switch Control 86100D-7FP 40S
OIF CEI Compliance Switch Control N1012A-7FP CES
SFF-8431 Measurement Suite Switch Control N1014A-7FP SFS
User Defined Application Switch Control N1019A-7FP MYS
IEEE 802.3 Compliance Switch Control N10812/3/4/5A-7FP IES
PAM4 Switch Option for Ethernet and OIF-CEI App N1085A-7FP PMS
Footnotes:
1. Characters that identify a feature in the string returned by the *OPT? common programming query.