N1010100A R&D Package
The N1010100A Research and Development Package License (L-RND) includes features optimized for using the DCA-X in a research and development environment.
This package enables the Research and Development Package features which are identified in the yellow column (L-RND) of the following table. If an L-RND feature is also offered in another package, a bullet is also shown for that package. However, the L-MFG and L-SNT columns only show shared features.
When installed, the remote *OPT?
query returns a comma-delimited string that includes the L-RND
field.
FlexDCA Features in R&D License Package
This table shows all the available features for the L-RND license package in the column with the highlighted yellow background. If a feature is also available in another package license, this is marked in non-highlighted columns.