N1010300A Signal Integrity Package

Package License:
L-SNT
Flex Apps:
FlexDCA
FlexPLL

The N1010300A Signal Integrity Package License (L-SNT) includes features optimized for using the DCA-X in a signal integrity environment.

This package enables the Signal Integrity Package features which are identified in the yellow column (L-SNT) of the following table. If an L-SNT feature is also offered in another package, a bullet is also shown for that package. However, the L-RND and L-MFG columns only show shared features.

When installed, the remote *OPT? query returns a comma-delimited string that includes the L-SNT field.

FlexDCA Features in Signal Integrity License Package

This table shows all the available features for the L-SNT license package in the column with the highlighted yellow background. If a feature is also available in another package license, this is marked in non-highlighted columns.

Feature OPT?1 Package Licenses
L-RND L-MFG L-SNT
Automatic Fixture Removal in TDR Mode F-AFR
Enhanced Impedance and S-Parameters F-ATDR
FlexDCA Remote Access Software F-FLEX
Data Analytics Web Service Software
As of FlexDCA revision A.06.02, a FlexDCA license is no longer required for this feature.
F-KAP
FlexPLL application that measures Jitter Transfer Function on devices with a PLL. F-PLL
User Defined Measurements and Operators F-UDMO
Footnotes:
1. Characters that identify a feature in the string returned by the *OPT? common programming query.