Last updated: December 2, 2008
Test set information is returned from a *IDN? query. The *IDN? query provides information about the Manufacturer, Model Number, Serial Number, and Firmware Revision. *IDN? is defined in IEEE Std. 488.2-1992, 10.14.
*IDN? query returns identification information as a comma separated string.
DIM A$[100] OUTPUT 714;"*IDN?" !returns manufacturer,model number, serial number and "0" !separated by commas ENTER 714;A$ PRINT A$ !prints, for example "Agilent Technologies, 8960 Series 10 E5515B, !US38020105,0
NOTE |