Last updated: December 2, 2008
Function |
This query returns the bad frame indication measurement results. The integrity indicator, number of samples counted, number of undetected bad frames, number of SIDs reported as bad frames, and the number of SIDs sent are returned. |
|
EGPRS LA | ||
GSM TA | ||
This command is not applicable to GPRS. | ||
This command is not applicable to EGPRS. | ||
|
||
Requirements | GSM/GPRS/ EGPRS LA |
Function | This query returns the number of undetected bad frames. | |
EGPRS LA | ||
GSM TA | ||
This command is not applicable to GPRS. | ||
This command is not applicable to EGPRS. | ||
Requirements | GSM/GPRS/ EGPRS LA |
Function |
This query returns the number of SIDs reported as bad frames. |
|
EGPRS LA | ||
GSM TA | ||
This command is not applicable to GPRS. | ||
This command is not applicable to EGPRS. | ||
Requirements | GSM/GPRS/ EGPRS LA |
Function | Queries the intermediate count (measurement progress report) of samples. | |
EGPRS LA | ||
GSM TA | ||
This command is not applicable to GPRS. | ||
This command is not applicable to EGPRS. | ||
Requirements | GSM/GPRS/ EGPRS LA |
Function |
This query returns the integrity indicator value for the last bad frame indication measurement performed. Zero indicates a normal result. See Integrity Indicator for descriptions of non-zero integrity indicators. |
|
EGPRS LA | ||
GSM TA | ||
This command is not applicable to GPRS. | ||
This command is not applicable to EGPRS. | ||
Range: See Integrity Indicator . |
||
Requirements | GSM/GPRS/ EGPRS LA |
Function | ||
EGPRS LA | ||
GSM TA | ||
This command is not applicable to GPRS. | ||
This command is not applicable to EGPRS. | ||
Requirements | GSM/GPRS/ EGPRS LA |