Last updated: December 2, 2008
Function |
This command sets/queries the number of samples to be taken by the FACCH frame erasure error (FER) measurement for the specified band. The FER sample number is a frequency banded parameter. Refer to Frequency Banded Parameters for a detailed description of the implications of being a banded parameter. |
|
EGPRS LA | ||
GSM TA | ||
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
Setting | ||
*RST Setting | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"SETup:FFERate:SAMPles 55000" ! Sets the number of samples to measure to 55000. |