Last updated: December 2, 2008
The Broadcast Allocation (BA) table in the test set provides a list of (P)BCH ARFCNs for each band that the mobile station must measure. This provides a means for you to stress the mobile station's receiver, especially when the traffic channel and the (P)BCH are in different bands. You can:
NOTE |
The BCH BA Table allows you to configure 32 BCH GSM neighbours cells. You can set the ARFCN(channel), BCC, NCC, Reporting Priority, and State for each Neighbour Cell.
The GPIB commands to configure the Neighbour Cell parameters in the BCH BA Table are as follows:
The parameters of each enabled Neighbour Cell in the BCH BA Table are broadcast in the System Information (SI) messages. Settings to the neighbour cell parameters are stored, but not applied until the neighbour cell is enabled.
The default value of the ARFCN for each BCH GSM neighbour cell depends on the selected broadcast band:
Band | Default ARFCNs (BCH GSM neighbour cell 1 to 32) |
---|---|
P-GSM | 20, 1, 62, 124, 9, 18, 36, 45, 54, 63, 72, 81, 90, 99, 108, 117, 7, 14, 21, 28, 35, 42, 49, 56, 63, 70, 77, 83, 91, 97, 104, 111 |
E-GSM | 20, 975, 37, 124, 986, 1008, 1019, 7, 18, 30, 53, 64, 76, 87, 99, 110, 10, 21, 30, 40, 50, 60, 70, 80, 90, 100, 111, 120, 980, 990, 1000, 1010 |
DCS | 512, 698, 885, 537, 562, 587, 612, 637, 662, 712, 737, 762, 787, 812, 837, 862, 525, 538, 551, 564, 577, 590, 603, 616, 629, 642, 655, 668, 681, 694, 707, 720 |
PCS | 512, 660, 810, 530, 550, 570, 590, 610, 630, 650, 690, 710, 730, 750, 770, 790, 531, 548, 566, 584, 602, 620, 638, 656, 674, 692, 711, 728, 746, 764, 782, 800 |
GSM850 | 150, 128, 190, 251, 138, 148, 158, 168, 178, 188, 198, 208, 218, 228, 238, 248, 135, 142, 149, 156, 163, 170, 177, 184, 191, 198, 205, 212, 219, 226, 233, 240 |
R-GSM | 20, 955, 28, 124, 969, 984, 999, 1014, 5, 21, 35, 50, 65, 80, 95, 110, 12, 24, 36, 48, 60, 72, 84, 96, 108, 120, 966, 977, 988, 1000, 1011, 1023 |
GSM450 | 270, 259, 276, 293, 262, 264, 267, 269, 272, 275, 277, 280, 282, 285, 287, 290, 260, 262, 264, 266, 268, 270, 273, 274, 276, 278, 280, 283, 284, 286, 288, 292 |
GSM480 | 310, 306, 323, 340, 309, 311, 314, 316, 319, 321, 324, 327, 329, 332, 334, 337, 308, 310, 312, 314, 317, 318, 320, 322, 325, 326, 328, 330, 333, 335, 336, 338 |
GSM750 | 450, 438, 474, 511, 444, 449, 454, 459, 465, 470, 476, 481, 487, 493, 499, 505, 442, 446, 450, 454, 458, 462, 466, 471, 475, 478, 482, 486, 490, 494, 498, 504 |
T-GSM810 | 380, 350, 388, 425, 356, 362, 367, 373, 379, 384, 390, 396, 401, 407, 413, 418, 354, 358, 363, 366, 370, 374, 378, 382, 386, 391, 394, 398, 402, 406, 410, 414 |
The BCH BA Table can also be configured manually by doing the following steps:
Cell Info
(
F6
).
Cell Lists
(
F4
).
GSM Neighbours (BCH)
(
F1
).The PBCCH BA Table allows you to configure 32 PBCCH GSM neighbour cells. You can set the ARFCN, BCC, NCC, RAC, Reporting Priority, and State for each Neighbour Cell.
The GPIB commands to configure the Neighbour Cell parameters in the PBCCH BA Table are as follows:
The parameters of each enabled Neighbour Cell in the PBCCH BA Table are broadcast in the Packet System Information (PSI) messages. Settings to the neighbour cell parameters are stored, but not applied until the neighbour cell is enabled.
NOTE: PSI messages are only transmitted when the Packet Broadcast Control Channel (PBCCH) is enabled.
The default value of the ARFCN for each PBCCH GSM neighbour cell is:
Default ARFCNs (PBCCH GSM neighbour cell 1 to 32) | |
---|---|
PBCCH BA Table | 20, 1, 62, 124, 9, 18, 36, 45, 54, 63, 72, 81, 90, 99, 108, 117, 7, 14, 21, 28, 35, 42, 49, 56, 63, 70, 77, 83, 91, 97, 104, 111 |
You can also control these parameters via the test set's front panel. The following procedure explains how to access the menus that allow you to configure simulated Neighbour Cell parameters that are transmitted on the PBCCH, when available. The Neighbour Cell menus are located in the Cell List menu.
Cell Info
(
F6
).
Cell Lists
(
F4
).
GSM Neighbours (PBCCH)
(
F2
).NOTE: You must enable the neighbour cell (set the State parameter to On), before you can access the other neighbour cell parameters.
NOTE: Since these parameters are sent on the PBCCH, these settings only apply the PBCCH state is On. See Packet Broadcast Control Channel (PBCCH) for more details.
The GPIB commands to configure general measurement reports parameters in the (P)BCH BA Table are as follows:
The general measurement reports parameters can also be configured manually by doing the following steps:
Control
menu to (
2 of 3
).
Measurement Reports
(
F6
).
Configure
(
F2
).
General Meas Parameters
(
F1
)