HTTP Interface for SMS - Introduction

HTTP Interface for SMS - Introduction

Last updated: December 3, 2008

This section is only applicable to lab applications and the test application with a required feature license.

The HTTP interface in the test set provides an industry standard interface for interfacing the base station simulation capability of the test set with necessary external components for verifying SMS capability in a mobile station. The HTTP implementation in the test set also provides SMS routing capability, simulating a simple Short Message Service Center (SMSC).

Introduction to HTTP

HTTP is the client/server based protocol used to deliver virtually all files and data on the World Wide Web. If you'd like a more detailed description of HTTP protocol, refer to Internet RFCs `HTTP/1.0 - RFC 1945' and `HTTP/1.1 - RFC 2616', which can be downloaded from http://www.rfc-editor.org/rfc.html.

When you use HTTP in a web browser, you enter the "address" for the web page you wish to view. These addresses can be generalized into the following format:

In this example, the web browser is the HTTP client and it uses the information in this address to open a connection to an HTTP server and send a request.

HTTP Interface for SMS verification

The test set acts as both a server and a client, depending on which operation it is performing.

The test set as the server:

If you have a PC and your test set connected to a network or directly connected together, you can open a web browser (client) and send a request to the test set using the test set's IP address and a correctly configured request URL. For example, you might send the following from the web browser if your test set's IP address was 111.111.111.112.

   
NOTE
It is not necessary to specify a port number because the test set uses 80, which is the default port for HTTP.

   

Sending the URL causes an SMS message to arrive at the mobile station attached to the test set's RF port. This message contains the text "hello".

The test set acts as the server for mobile terminated SMS messages. While this is a simple example, this same information is necessary to configure an SMS Gateway or proprietary software for interfacing with the test set via HTTP.

For configuration information see:

The test set as the client:

SMS messages originating from the mobile station attached to the test set are sent out the test set's LAN port as HTTP requests to the IP address for the intended receiving entity.

For configuration information see:

Related Topics


HTTP Interface Configuration for Mobile Terminated SMS

HTTP Interface Configuration for Mobile Originated SMS

HTTP SMS Router Web-based Configuration Interface