Last updated: December 3, 2008
This section is only applicable to lab applications and the test application with a required feature license.
This section explains how to use the web-based interface provided for configuring the HTTP SMS Router for mobile originated SMS messages. To configure the HTTP Interface for Mobile Originated SMS, you must have an active LAN connection to the test set in order to access its http server. You can access the HTML pages for configuration via any standard internet browser.
HTTP SMS Router Current Configuration
page. The current HTTP Interface Settings are summarized on the Current Configuration page. See Change Configuration for information on changing these settings.
NOTE |
The following parameters are configured using the HTTP SMS Router Web-based Configuration Interface. For more detailed explanation of each of these parameters, see HTTP Interface Settings - General .
Click on the Change button from the
HTTP SMS Router Current Configuration
page to access the
HTTP SMS Router Change Configuration
page.
The
HTTP SMS Router Change Configuration
page, shown in the figure below, allows changes to be made to the HTTP Interface Settings.
The HTTP SMS Router Change Configuration page is divided into two sections: General and Output Destination.
This section controls the number that is associated with the mobile station for messages output over the HTTP interface.
This section allows you to specify the destination for mobile originated SMS messages. If this is another test set, only the IP address of the destination test set is required for this section. For other destinations, such as an SMS Gateway running on a PC, more specific details are required.
Click the
Apply Changes
button to save any configuration changes you have made. The browser returns to the
HTTP SMS Router Current Configuration
page.
Alternatively, use the
Cancel
button to discard any changes you have made that you do not want saved.
If any of the settings specified on the
page contain illegal values when the
HTTP SMS Router Change Configuration
Apply Changes
button is clicked, the
HTTP SMS Router Configuration Error
page is displayed. This page provides a description of the first error found when verifying the updated settings. Press the
Back
button to return to the
HTTP SMS Router Change Configuration
page to correct any errors.
HTTP Interface Configuration for Mobile Originated SMS