Last updated: December 3, 2008
This section is only applicable to lab applications and the test application with a required feature license.
If you wish to use the HTTP interface in the test set to route SMS messages to the mobile station attached to the test set's RF port you must do the following:
You must enable the HTTP interface in the test set. This can be done via a GPIB command (see CALL:SMService:HTTProtocol:INPut ) or from the test set's front panel (see Enabling the HTTP Interface for Mobile Terminated SMS ).
If the interface is not enabled, HTTP SMS requests sent to the test set are rejected and the HTTP error code 503 (Service Unavailable) is returned to the client issuing the request.
Several different types of clients could be used to send SMS messages to the test set. Some examples are:
When setting up any of these clients, it is necessary to specify the IP Address and port number on which the test set is listening for incoming messages. These parameters are always to be configured as follows:
NOTE |
When using the HTTP interface in the test set for sending SMS messages, you must configure a request URL.
Requests to send SMS messages to the mobile station attached to the test set using the HTTP interface must be configured using the following rules:
/sms/send/?parameter1=value1¶meter2=value2¶meter3=value3......
NOTE |
The parameters and values variables provides the content of the SMS message as well as additional information for header configuration and test set configuration. All configurable parameters and values are detailed in Request URL Parameters .
SMS Message Content Type | Mandatory Parameters |
---|---|
7-bit text | TEXT |
8 or 16 bit data | DATA and/or UDH |
Optional Parameters |
---|
UDHI |
PIDHEX or PID |
DCSHEX or DCS |
SENDER |
MMTS |
SRI |
RPATH |
TRANSPORT |
NOTE |
To send a text based SMS message with the following message details:
you would format the HTTP request URL as follows:
/sms/send/?TEXT=This%20is%20a%20simple%20text%20message&SENDER=1001
To send a binary message with the following message details:
you would format the HTTP request URL as follows:
/sms/send/?DATA=140601AE02056A0045C60D036262632E636F2E756B2F6D6F62696C6500070103424243206D6F62696C652073697465000101&PID=0&DCS=245&SENDER=987654321&UDH=0605040B8423F0
or, the test set also allows you to include the User Data Header as part of the `DATA' parameter as explained in the table Request URL Parameters . Therefore, the HTTP request URL could instead be configured as follows:
/sms/send/?DATA=0605040B8423F0140601AE02056A0045C60D036262632E636F2E756B2F6D6F62696C6500070103424243206D6F62696C652073697465000101&UDHI=1&PID=0&DCS=245&SENDER=987654321
Both POST and GET HTTP requests are accepted by the test set for sending SMS messages.
If POST is used as the request method, the URL request parameters detailed in Request URL Parameters are not included in the request URL, but are included in the request body instead. Therefore, the request URL in POST requests contains only `sms/send'.