Last updated: December 3, 2008
GSM TA | This command is not applicable to the GPRS test application. | |
This command is not applicable to the GPRS test application. | ||
This command is not applicable to the EGPRS test application. | ||
Command the test set to start playing the digital audio file. See Digital Audio Interface (DAI) Description for more information. | ||
GSM/GPRS/ EGPRS TA | ||
OUTPUT 714;"CALL:DAINterface:PLAY:STARt" ! Commands the test set to start playing the digital audio file. |
GSM TA | This command is not applicable to the GPRS test application. | |
This command is not applicable to the GPRS test application. | ||
This command is not applicable to the EGPRS test application. | ||
This command queries the playing status of the digital audio file in the test set. See Digital Audio Interface (DAI) Description for more information. |
||
GSM/GPRS/ EGPRS TA | ||
OUTPUT 714;"CALL:DAINterface:PLAY:STATus?" ! Queries the playing status of the digital audio file. |
GSM TA | This command is not applicable to the GPRS test application. | |
This command is not applicable to the GPRS test application. | ||
This command is not applicable to the EGPRS test application. | ||
Command the test set to stop playing the digital audio file. See Digital Audio Interface (DAI) Description for more information. | ||
GSM/GPRS/ EGPRS TA | ||
OUTPUT 714;"CALL:DAINterface:PLAY:STOP" ! Commands the test set to stop playing the digital audio file. |
GSM TA | This command is not applicable to the GPRS test application. | |
This command is not applicable to the GPRS test application. | ||
This command is not applicable to the EGPRS test application. | ||
This command sets/queries the type of the digital audio file in the test set. See Digital Audio Interface (DAI) Description for more information. |
||
GSM/GPRS/ EGPRS TA | ||
OUTPUT 714;"CALL:DAINterface:RECord:FORMat:AMR COD" ! Sets the type to COD. |
GSM TA | This command is not applicable to the GPRS test application. | |
This command is not applicable to the GPRS test application. | ||
This command is not applicable to the EGPRS test application. | ||
Command the test set to start recording the digital audio file. See Digital Audio Interface (DAI) Description for more information. | ||
GSM/GPRS/ EGPRS TA | ||
OUTPUT 714;"CALL:DAINterface:RECord:STARt" ! Commands the test set to start recording the digital audio file. |
GSM TA | This command is not applicable to the GPRS test application. | |
This command is not applicable to the GPRS test application. | ||
This command is not applicable to the EGPRS test application. | ||
This command queries the recording status of the digital audio file in the test set. See Digital Audio Interface (DAI) Description for more information. |
||
GSM/GPRS/ EGPRS TA | ||
OUTPUT 714;"CALL:DAINterface:RECord:STATus?" ! Queries the recording status of the digital audio file. |
GSM TA | This command is not applicable to the GPRS test application. | |
This command is not applicable to the GPRS test application. | ||
This command is not applicable to the EGPRS test application. | ||
Command the test set to stop recording the digital audio file. See Digital Audio Interface (DAI) Description for more information. | ||
GSM/GPRS/ EGPRS TA | ||
OUTPUT 714;"CALL:DAINterface:RECord:STOP" ! Commands the test set to stop recording the digital audio file. |