Last updated: December 3, 2008
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This command sets/queries the Daylight Saving Time value. See Network Identity and Time Zone for more information. | |
EGPRS LA | ||
0 | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:NITZone:DSTime:TDMA 0" !Sets the daylight saving time to 0. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This command sets/queries whether the Network Daylight Saving Time Information Element is included in the GMM or MM Information message or not. See Network Identity and Time Zone for more information. | |
EGPRS LA | ||
Range: ON|OFF|1|0 | ||
Range: 1|0 | ||
OFF | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:NITZone:DSTime:STATe:TDMA OFF" ! !Sets the GMM or MM info message do NOT include daylight saving time Information Element. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This command sets/queries the Daylight Saving Time value. See Network Identity and Time Zone for more information. | |
EGPRS LA | ||
0 | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:NITZone:DSTime:VALue:TDMA 0" !Sets the daylight saving time to 0. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command sets the NITZ Information to be immediately sent to the mobile when:
See Network Identity and Time Zone for more information |
|
EGPRS LA | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:NITZone:SEND" !Sets the NITZ information to be immediately sent to DUT via GMM Information message. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command sets/queries whether the NITZ information is sent during a GPRS PDP activation procedure and Point-to-Point SMS over GPRS procedure. When this parameter is set to ON, the GMM Information message with NITZ information is sent following these messages:
See Network Identity and Time Zone for more information |
|
EGPRS LA | ||
Range: ON|OFF|1|0 | ||
Range: 1|0 | ||
OFF | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:NITZone:SEND:DATA:ORIGination:TDMA OFF" !Sets the test set does NOT send GMM information message during a GPRS PDP activation procedure and Point-to-Point SMS over GPRS procedure. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command sets/queries whether the NITZ information is sent during a GPRS Attach procedure and Routing Area Update procedure. When the parameter is set to ON, the GMM Information message with NITZ information is sent following these messages: See Network Identity and Time Zone for more information |
|
EGPRS LA | ||
Range: ON|OFF|1|0 | ||
Range: 1|0 | ||
OFF | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:NITZone:SEND:GMM:REGistration:TDMA OFF" ! !Sets the test set does NOT send GMM information message during a GPRS Attach procedure or Routing Area Update procedure. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command is not applicable to the EGPRS Test Application. |
|
EGPRS LA |
This command sets/queries whether the NITZ information is sent during IMSI Attach procedure and Location Updating procedure. When this parameter is set to ON, the MM Information message with NITZ information is sent following the message listed: See Network Identity and Time Zone for more information |
|
Range: ON|OFF|1|0 | ||
Range: 1|0 | ||
OFF | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:NITZone:SEND:MM:REGistration:TDMA OFF" !Sets the test set does NOT send NITZ information during IMSI Attach procedure and Location Updating procedure. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command sets/queries which message (MM Information or GMM Information) is used to transport NITZ information after "NITZ Send Immediate" setting is applied, in the cases where both GMM Infomation and MM Information messages are available. (For example, in a DTM operation.) If the parameter is set to GSM, NITZ information is sent via MM Information message, otherwise it is sent via GMM Information message. See Network Identity and Time Zone for more information |
|
EGPRS LA | ||
GPRS | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:NITZone:SEND:TRANsport:TDMA GPRS" ! !Sets the NITZ information to be sent via GMM Information message. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command sets/queries whether the NITZ information will be sent or not during a voice call origination procedure (including voice, emergency call and CSD) and Point-to-Point SMS over GSM procedure. When this parameter is set to ON, the MM Information message with NITZ information is sent following the messages listed: CM Service Accept message from the test set during a mobile originated call for voice, CSD, emergency call and Point-to-Point SMS over GSM
See Network Identity and Time Zone for more information |
|
EGPRS LA | ||
Range: ON|OFF|1|0 | ||
Range: 1|0 | ||
OFF | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:NITZone:SEND:VOICe:ORIGination:TDMA OFF" !Sets the test set does NOT send MM information message during a voice call origination procedure and Point-to-Point SMS over GSM procedure. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command sets/queries the NITZ local time zone. The format of entry is hh.mm and the resolution is 15 minutes. Thus, any entry that does not fall evenly on a 15 minute (quarter hour) boundary will be rounded to the nearest 15 minutes. See Network Identity and Time Zone for more information |
|
EGPRS LA | ||
"00.00" | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:NITZone:TZONe:TDMA 00,00" !Sets the local time zone to 00.00 |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This command sets/queries the Universal Time-Date. The format of entry is yyyy.mm.dd. See Network Identity and Time Zone for more information. | |
EGPRS LA | ||
"2008.01.01" | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:NITZone:UTIMe:DATE:TDMA 2008,01,01" !Sets the date to January 1,2008. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This command sets/queries the Universal Time-Time. The format of entry is hh.mm.ss using the 24-hour clock. See Network Identity and Time Zone for more information. | |
EGPRS LA | ||
Note that the resolution of the local time setting is minutes. The value returned for <second> will not provide useful information. |
||
"13.00.00" | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:NITZone:UTIMe:TIME:TDMA 13,00,00" !Sets the universal time to 13:00. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This command sets the NITZ Universal Time and Date to the Universal Coordinated Time and Date as found on the System Configuration Screen. See Network Identity and Time Zone for more information. | |
EGPRS LA | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:NITZone:UTIMe:UTC" |