Last updated: December 3, 2008
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Sets/Queries the Packet Flow Context (PFC) State. When the Packet Flow Context state is set to ON, You can set the Packet Flow Identifier (PFI) for each QoS Profile using the GPIB command CALL:PPRocedure[:QOSProfile[1]|2|3|4]:PFI . Note: The Operating Mode must be set to Cell Off before setting this parameter. See CALL:OPERating for more details. |
|
EGPRS LA | ||
Range: 1|ON|0|OFF | ||
OFF | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:PFCONTEXT ON" ! Sets the Packet Flow Context State to ON. |