Last updated: December 3, 2008
This command is not applicable to the GSM test applications. | ||
GPRS TA | This command is not applicable to the GPRS test applications. | |
EGPRS TA | This command is not applicable to the EGPRS test applications. | |
GSM/GPRS LA |
This command sets the list of equivalent PLMNs. See Equivalent PLMN List for more information. |
|
EGPRS LA | ||
Setting | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PLMNetwork 1,3,7,9,55,32,55,87,654,525,5,54,88,56,26,4,8,56,25,42,22,666,545,222,88,56,5,9,5,2" ! The test set the list of equivalent PLMNs to {1,3,7,9,55,32,55,87,654,525,5,54,88,56,26,4,8,56,25,42,22,666,545,222,88,56,5,9,5,2}". |