CALL:PPRocedure:LAU|LAUPdate

CALL:PPRocedure:LAU|LAUPdate

Last updated: December 3, 2008

GPIB Command Conventions

CALL:PPRocedure:LAU|LAUPdate:REJect[:STATe]

Function

GSM TA

This command is not applicable to the GSM test applications.
GPRS TA This command is not applicable to the GPRS test applications.
EGPRS TA This command is not applicable to the EGPRS test applications.
GSM/GPRS LA

This command sets Location Area Update Reject State. When the parameter is set to ON, the test set will reject the LAU request from the mobile station.

EGPRS LA
Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST setting

0|OFF

Requirements

GSM/GPRS/ EGPRS LA

Revision: F.00.27 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:LAUPdate:REJect:STATe ON" 
! Sets the Location Area Update Reject State to ON.

CALL:PPRocedure:LAU|LAUPdate:REJect:GMMCause

Function

GSM TA

This command is not applicable to the GSM test applications.
GPRS TA This command is not applicable to the GPRS test applications.
EGPRS TA This command is not applicable to the EGPRS test applications.
GSM/GPRS LA

This command sets the Location Area Update Reject cause.

See GMM Cause Information Element for details on settings this parameter accepts as defined in 3GPP TS 24.008 Version 6.7.0.

EGPRS LA
Setting

Range: 0 to 255 (decimal)

Query

Range: 0 to 255

*RST setting

+12

Requirements

GSM/GPRS/ EGPRS LA

Revision: F.00.27 and above

Programming Example:

 
OUTPUT 714;"CALL:PPRocedure:LAUPdate:REJect:GMMCause 3" 
! The test set sends the MS the RAU Reject cause value as "Illegal MS".

CALL:PPRocedure:LAU|LAUPdate:T3212

Function

GSM TA

This command is not applicable to the GSM Test Application.
GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

GSM/GPRS LA

Sets the Periodic Location Update Timer value. See Configurable Timers .

EGPRS LA
Setting

Range: 0 to 255 (decihours)

Query

Range: 0 to 255 (decihours)

*RST setting

0

Requirements

GSM/GPRS/ EGPRS LA

Revision: F.00.27 and above

Programming Example:

 
OUTPUT 714;"CALL:PPROCEDURE:LAU:T3212 20" 
! Set the expire time of T3212 to 2 decihours (12 minutes).